Creating A Growing Market For Air Quality Sensors | Avnet Abacus

Display portlet menu

How sensitivity to our environment is creating a growing market for air quality sensors

A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality. There’s even a London web site dedicated to providing information about air pollution in the city and of course and inevitable smartphone app to keep you up to date with the facts on how quickly you’re being poisoned. Yes, air pollution and mortality rate are closely linked. Public Health England (PHE) published a report in April 2014 that estimated the number of deaths in UK local authorities attributable to long term exposure to man-made particles less than 2.5 microns in diameter. It concluded that 8% of deaths in London (and possibly almost double this number) could be attributed to long-term exposure to particulate pollution – most of which is created by motor vehicles. All cities suffer from this kind of pollution, some more than others, depending on traffic density, other sources of particulates, weather conditions and various geographic factors.

However, particulates are not the only pollutants that damage health. Carbon monoxide (CO), excess levels of carbon dioxide (CO2), and high concentrations of gases such as propane or methane also have adverse, and sometimes fatal consequences for humans. 

Some air conditioners in offices and homes no longer just operate on the basis of controlling temperature. Smart sensors also take account of humidity, particulates of various sizes and even the presence of tobacco smoke.

One US company, Sensorcon, developed a multi-sensor tool, called Sensodrone, for use with a smartphone. Funded through KickStarter, the firm describes the product as “the world’s first mobile, wearable, programmable sensing computer” and one journalist described it as “a Swiss Army Knife of environmental input.” 

Sensodrone incorporates a carbon monoxide detector, non-contact thermometer, gas leak detector, lux meter, weather station, diagnostic tool, breath analyser and more. 

 

The much-vaunted Internet of Things will involve billions of sensors from which data is processed and communicated, and new products that control and safeguard our environment will be developed in their droves over the next few years. Here are just a few examples of CO2, humidity and temperature sensors.

Amphenol air quality sensors include The Telaire T6613/66715 series of modules for CO2 detection (right). They come in single and dual channel versions and there are complementary duct-mount or wall-mount transmitters. Humidity and temperature models of the wall-mount versions are available too. Accurate sensing results in well-controlled environments in which energy consumption is minimised, realising considerable cost savings.

Alps humidity sensors are used in everything from home appliances to health care devices. Various versions provide absolute or relative humidity measurement based upon changes in the mechanical or electrical state of hygroscopic materials inside the devices. The most popular type, the HSHCA, translates changes in humidity to changes in capacitance to produce a highly linear response without the need for temperature compensation circuits. The Alps HTUD sensor is a plug-and-play device that combines humidity and temperature sensing in one compact, DFN package.

Amphenol EMD-4000 sensors are resistive devices for measuring relative humidity. They’re used in air conditioning systems for commercial premises, homes and automobiles and have a measurement range of 20% to 95% relative humidity at 25 °C.

TDK also uses resistive humidity sensing in its CHS family of humidity sensors. The products are particularly resistant to the ingress of water and various gases, and exhibit no hysteresis when measuring between 5% and 95% relatively humidity levels.

   

Hygrometers and air humidifiers are the primary applications for capacitive atmospheric humidity sensors from Vishay. Each sensor consists of a non-conductive foil, which is covered on both sides with a layer of gold. The dielectric constant of the foil changes as a function of the relative humidity of the ambient atmosphere and, accordingly, the capacitance value of the sensor is a measure of relative humidity. Relative humidity from 10% to 90% is measured and the devices can be used from 0 to 85 °C, a wider temperature range than most of the resistive types.

Humidity sensors and humidity/temperature sensor modules (left) are also made by TE Connectivity (formerly Measurement Specialties). These sensors employ a unique capacitive cell for humidity measurement and a Negative Temperature Coefficient (NTC) thermistor for temperature measurement. They’re useful in applications where dew point, absolute humidity measurements or humidity compensation are required. 

 

 

These are just a few examples of sensors available from Avnet Abacus. If you need help in selecting the best one for your application, please get in touch using our Ask an Expert page.

Written by

Giovanna Monari 

Senior Product Manager, Electromechanical, EMEA

Creating A Growing Market For Air Quality Sensors | Avnet Abacus

Display portlet menu

RELATED ARTICLES

A quick guide to powering smart objects with kinetic energy harvesting

As the world becomes increasingly smart and connected, batteries can be undesirable in some of the u...

From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica

And so electronica 2018 is over. In our final post, we look back on the best bits of day three....

electronica 2018 day two highlights

Another day at electronica 2018 has passed and it was arguably even busier than the first. A constan...

Engineering Services

Ask an expert

Have a question? Our regional technical specialists are on hand to help