Modern Electromechanical Relay For Today’S Demands | Avnet Abacus

Display portlet menu

Modern electromechanical relays meet today’s reliability demands

Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer. Of all the relay types, they are probably the best general-purpose solution, meeting the needs of many diverse applications from automotive to automated test equipment. Many, many different specialist types of EMRs exist for everything from signal transmission to power electronics applications. These days, they are often specified purely for cost reasons, but they do have some redeeming features. 

EMRs are mechanical devices that physically open and close electrical contacts when they are switched on and off. This means they have a very low contact resistance – in the tens of milliohms – which is important for applications that require a minimal on-state voltage drop. They also offer very high open resistance – typically greater than 100 GΩ. Contact capacitance is also less than what’s offered by SSRs, which means they can offer the linear response that’s required to minimise distortion of high frequency signals, and they have high bandwidth characteristics (>100MHz).

Applications that require Galvanic isolation between the drive electronics and the relay contacts will make use of the EMR’s ability to provide nearly total line to load isolation. Even multiple pole devices, which can control multiple circuits at the same time, are fully isolated. 
EMRs’ contacts are large and robust, so they can withstand power surges and voltage spikes. Transients under some circumstances can switch SSRs, whereas this isn’t a problem for EMRs. SSRs also have a tendency to fail in short circuit mode, which can lead to damage for the equipment or circuits being switched on or off.

Of course, there are down sides to using EMRs. Audible noise is one, followed by limitations on switching speed (5 to 15ms) and their general bulkiness. There are many application areas where these criteria are less important than cost, or the EMR’s other features such as surge resistance, so it’s a matter of matching the strengths of the relay type to the application’s requirements. 

Life expectancy, in particular, is often thought of as relatively low for EMRs, but in fact this is one property of EMRs that manufacturers have been working on in recent years. Since they are mechanical components, they have a finite lifetime, referred to as endurance, which begins when the relay is first switched. Endurance is usually defined in terms of how many switching operations the relay can be expected to perform under certain conditions before failure. 

EMR datasheets typically give both the mechanical and electrical endurance figures. Mechanical endurance is a measure of the number of cycles of operation a relay can be expected to perform with no electrical load. The electrical endurance gives the expected number of cycles of operation before failure under a certain electrical load. Endurance is sometimes separated for AC and DC loads if the relay is suitable for use with both. Note that mechanical and electrical endurance have different failure criteria – that is, they are not comparable. Mechanical endurance is therefore not a good approximation for electrical endurance under low load conditions. 

Typical conditions under which electrical endurance is measured include relay duty factor of 50% at rated frequency and rated voltage, with a resistive load, at ambient temperature (23°C), with the relay upright, wired directly (not mounted on a socket), with the contact opening/closing not synchronised to line frequency, etc. Of course, if your application demands conditions different to these standard test conditions, some level of derating can be expected. 

Here are some examples of modern EMRs and their failure rates.

The Omron MY series on the image right includes a broad range of general-purpose relays. The MY2 series of miniature power relays offers mechanical endurance of 50 million operations minimum when used with an AC load, or 100 million operations minimum with a DC load. Its electrical resistance is 500,000 operations minimum at rated load, at rated switching frequency of 18,000 operations per hour.

The GQ series of signal relays from Panasonic Electric Works is rated for 2A signals. Their expected mechanical endurance is a minimum of 50 million operations when switched at 180 times per minute. Their electrical endurance with a 2A, 30VDC resistive load is 50,000 operations minimum at 20 times per minute, or 100,000 operations minimum at 20 times per minute for 1A, 30VDC resistive loads. For 0.3A, 125VAC resistive loads, a minimum of 100,000 operations at 20 times per minute can be expected. 

Electrical endurance of Panasonic Electric Works’ GQ series

 

TE Connectivity’s high current relay 150 is a much bigger relay intended for engine control, engine preheating systems, heated windscreens and other automotive applications. Its mechanical endurance is 10 million operations minimum, and its electrical endurance is 50,000 cycles minimum at 300A, 13.5VDC.

 

TE Connectivity’s high current relay 150 for automotive applications

 

Avnet Abacus works with market leading suppliers including Omron, Panasonic Electric Works and TE Connectivity to provide EMR components covering a broad range of specifications, giving you flexibility in any application. Our Europe-wide team of technical specialists are happy to discuss how EMR products could optimise your designs and answer any questions. Contact them in your local language through our Ask an Expert page.

 

 

Written by

Giovanna Monari 

Senior Product Manager, Electromechanical, EMEA

Modern Electromechanical Relay For Today’S Demands | Avnet Abacus

Display portlet menu

RELATED ARTICLES

A quick guide to powering smart objects with kinetic energy harvesting

As the world becomes increasingly smart and connected, batteries can be undesirable in some of the u...

From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica

And so electronica 2018 is over. In our final post, we look back on the best bits of day three....

electronica 2018 day two highlights

Another day at electronica 2018 has passed and it was arguably even busier than the first. A constan...

Engineering Services

Ask an expert

Have a question? Our regional technical specialists are on hand to help