Multi-Standard Mesh Networking

Display portlet menu

Multi-Standard Mesh Networking

Display portlet menu

A quick guide to multi-standard mesh networking

Alessandro Mastellari Photo

Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?


Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications. Low cost IoT technology is driving the launch of devices such as smart lighting systems, smart locks, smart thermostats, voice control products, smart alarms, garage door openers, smart fan control, smart plugs and many more.

Wireless Mesh Networks (WMN) are an ideal solution for these types of applications, offering cable-free, low-power and low-cost methods of connecting multiple devices within an area, such as a large single floor, multi-floor dwelling or office. The emergence of WMN protocols such as Zigbee, Thread and, more recently, Bluetooth, have further enhanced the appeal of WMNs, by simplifying the configuration and management of WMNs.
 

Wireless mesh networking

In a mesh topology the network nodes connect directly to as many other nodes as possible, cooperating with one another to route data across the network. This topology allows the creation of very large networks of interconnected, low-power devices and also has the advantage of being “self-healing” due to the multiple possible paths that data can take through the mesh. The exact functionality of the network nodes varies depending on the specific WMN (as shown in the table below) protocol but a node can either function as a network routing element, receiving and transmitting data bound for another node, an end-point device, such as a sensor, or a combination of both. A WMN will also include at least one gateway device, enabling connectivity beyond the mesh, e.g. for internet “backhaul”.

  Bluetooth Mesh Zigbee Thread
Established 2017 2002 2015
Mesh type Flooded mesh Routed mesh Routed mesh
Network size (theoretical limit) 32768 addressable elements. No limits on relay nodes Up to 65,000 1 leader, 32 routers, 511 per router end device
Security Confidentiality, authentication and key derivation AES encryption, cipher block chaining message authentication code Banking-class, public-key cryptography
Area Good for sensor networks, better for control; networks Better for sensor networks / control networks Better for sensor networks / control networks
Application focus Lighting, home automation Lighting, home automation, metering Commercial, industrial
Bandwidth 1Mbps 250kbps 250kbps
Payload size limit 251 Bytes 80 Bytes 1kB default, up to 64kB
Radio Bluetooth LE v4.0 (IEEE802.15.1), 2.4GHz IEEE802.15.4 PHY, 2.4GHz, 915MHz and 868MHz IEEE802.15.4 PHY, 2.4GHz
Power consumption Battery current <15mA Battery current 10-30mA Battery current 10-30mA
Distance Approximately 10 to 100m  Up to 300+m (line of sight) 20 to 30m

Comparison of Bluetooth Mesh/Zigbee/Thread

WMN protocols

Four main WMN protocols have emerged in recent years - Z-Wave, Zigbee, Thread, (based on 6LoWPAN) and, most recently, Bluetooth mesh. Each protocol has its own characteristics, such as maximum network size, throughput and latency, but all four support the creation of low-power, low-data networks and are ideal for home and building automation applications.

Zigbee, the most established, has the largest eco-system, including manufacturers such as Amazon Echo Plus, Philips Hue, Comcast Xfinity, IKEA and Samsung SmartThings. Thread’s legacy, based on its reputation for enhanced security levels, is in the industrial sector but, backed by Google, (through Nest Labs), and with organisations such as Apple joining the eco-system, the popularity of the protocol is set to grow.

As each protocol evolves, however, the performance differences between them are likely to decrease; Bluetooth mesh in particular is likely to quickly gain support due to the overwhelming number of manufacturers and devices using previous versions for classic point-to-point applications.
 

WMN application design considerations

One of the most important factors to be considered when choosing a protocol for an application is the eco-system. Based on its maturity and popularity, Zigbee has the most devices using the protocol, with a large library of pre-developed software available. Bluetooth’s eco-system, on the other hand, is potentially huge, due to its ubiquitous use in smart-phones, tablets, etc., and more and more Bluetooth mesh network applications are being developed. Bluetooth also has the benefit of being easier to scale for large networks.

Out of the three protocols, Thread is the only one based on IPv6, providing unique benefits, such as end-to-end routing and addressability on the same or across networks, without the need for additional translation layers to be implemented.

Other factors to consider include maximum network size, throughputs and latencies. Comparative studies show that all three perform similarly in small networks under small payloads with Bluetooth lagging the other two as payload and throughput needs increase. Whilst latency for all three protocols increases with network size, Bluetooth mesh latency increases the most.

A growing number of multi-protocol WMN modules is appearing on the market which brings inter-operability advantages and also enables network devices to combine functionality, such as the networking characteristics of Zigbee with the beaconing and direct control functionality of Bluetooth.
 

Taiyo Yuden EYSKBNZWB BLE wireless module

The Taiyo Yuden EYSKBNZWB, shown right, is an example of such a multi-protocol device, capable of running the Bluetooth 5.0 and 802.15.4 stacks concurrently, supporting Bluetooth as well as Zigbee or Thread and enabling interoperability between protocols. By acting as a gateway, the EYSKBNZWB enables newer devices running Bluetooth to be added to existing networks based on Zigbee or Thread. This gateway functionality simplifies the extension or upgrading of existing home or building networks as new devices and applications can easily be added without having to replace existing networks. The module also provides valuable end-user benefits by enabling smart phones to interact directly with network devices such as light bulbs, without the need for a multi-standard gateway. NFC is also supported by the EYSKBNZWB, which offers further pairing options as well as supporting applications such as smart locks.

The module is based on the Nordic nRF52840 chip and, as Nordic is the market leader in Bluetooth, application developers have access to an extensive library of pre-developed software. Although small, the EYSKBNZWB is a full spec Bluetooth 5.0 module with an onboard antenna and is unique in that it supports high data rates, up to 2Mbps, and long range, with output power up to +8dBm.
 

Summary

Three main WMN protocols have emerged as contenders for the smart home and building market, each with its own pros and cons, depending on the needs of the specific application. Multi-protocol modules such as the Taiyo Yuden EYSKBNZWB enable the developer to achieve inter-operability and also combine features of more than one protocol on a single device. Click here to request a sample and start testing your design.

Want more like this? Sign up for our newsletters

About Author

Alessandro Mastellari Photo
Alessandro Mastellari

Alessandro has over 20 years experience in the electronics industry, spanning product management and...

Multi-Standard Mesh Networking

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Multi-Standard Mesh Networking

Display portlet menu
Related Articles
Automation manufacture Industry 4.0
Evolution before revolution: the origins of Industry 4.0
May 27, 2020
We’ve come a long way from the days of Henry Ford famously telling customers that they could have the Model T car painted any colour ‘so long as it was black’ – a quote which reflected the compromise of having to put efficiency before choice.
Product
The evolution of cellular networks
By Martin Keenan   -   April 29, 2020
Since the first 5G services were launched in the USA by Verizon and AT&T, 5G networks have been rolled out in a further 17 countries with South Korea, the United Kingdom, Germany, and the United States leading the charge and China catching up fast.
Abstract image of an electronic circuit
How SiC and GaN technology is affecting passive component development
June 19, 2020
To keep up with the semiconductor process innovations, SiC and GaN present some unique challenges to the essential passive components used in power conversion and motor drive circuits.
Satellite in action around the Earth
The future is 5G
By Adam Chidley   -   April 29, 2020
'The explosive growth of the IoT shows no signs of abating, with Gartner forecasting 20.8 billion connected “things” by 2020, and IHS Markit predicting that this number will rise to 125 billion by 2030.'
A technical specialist on solar panels
Extending battery lifetime in wireless applications using supercapacitors
By Martin Keenan   -   April 20, 2020
This article describes how supercapacitors can be deployed in conjunction with batteries to extend their operational life and reduce maintenance and replacement costs.
Engineer using an oscilloscope to test a circuit
Selecting relays for test and measurement equipment
By Shlomo Avital   -   March 30, 2020
One of the key challenges with developing test and measurement equipment is to ensure that the signal that gets measured is the same as the signal that you want to measure. It sounds obvious, but multiple factors in the path from the test point to the me...
An electric vehicle charging cable being plugged into a charging station
An introduction to EV charging infrastructure design
February 7, 2020
With demand for faster charging of EV vehicles increasing, the design of charging stations and infrastructure becomes ever more important.
Inside of a connected car depicting
V2X: The future of vehicle communications
By Martin Keenan   -   December 10, 2019
Vehicles are about to become a lot more communicative: with other road users, with the infrastructure they pass on their journeys, with cloud-based services, and even with the energy grid. This communication should make vehicles more economical to operate...
A photo of various antennas laid out on a white background
4 keys to selecting antennas for small IoT devices
November 19, 2019
Wireless connectivity is a critical enabler for many IoT applications. While a wireless module can simplify the RF subsystem design, a working system requires careful selection of an antenna as well.
Tesla plugged into charging station
Switching high voltages and currents with PCB-mounted relays
By Martin Keenan   -   November 8, 2019
The growing demand for safe, robust and energy-efficient ways to switch relatively large amounts of power means that relays have an important role to play in a wide range of modern applications.
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
There are two primary technologies used in detecting the presence of people, pyro-electric / passive infra-red (PIR) and ultrasonic. Alessandro Mastellari takes a look at how they differ and how they work.
PIR and ultrasonic sensors: What's the difference and how do they work?
By Alessandro Mastellari   -   October 21, 2019
There are two primary technologies used in detecting the presence of people, pyro-electric / passive infra-red (PIR) and ultrasonic. Alessandro Mastellari takes a look at how they differ and how they work.
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
These 8 charts will challenge your perspective on the Industrial IoT
October 1, 2019
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
While connectors are not the most interesting components in automotive systems, they can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
4 factors steering connector choices in today's automotive applications
September 16, 2019
Connectors are critical components in any automotive systems, and their selection can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
A quick guide to powering smart objects with kinetic energy harvesting
By Alessandro Mastellari   -   January 22, 2019
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
Andy Hutton investigates the problems that LED flicker can cause in day-to-day life and the steps designers can take to prevent it in their lighting applications.
What is LED flicker - and how to prevent it
By Andrew Hutton   -   January 9, 2019
Andy Hutton investigates the problems that LED flicker can cause in day-to-day life and the steps designers can take to prevent it in their lighting applications.
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Design trends: Automotive passives
By Martin Keenan   -   November 29, 2018
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
ENEC (European Norms Electrical Certification) is the European hallmark for luminaires and related products and is used to demonstrate compliance with European safety standards. This certification system also includes LED drivers
Designing safe certified and efficient power solutions for LED lighting system
By Philip Lechner   -   November 22, 2018
ENEC (European Norms Electrical Certification) is the European hallmark for luminaires and related products and is used to demonstrate compliance with European safety standards. This certification system also includes LED drivers - the electronics th
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
Key design considerations for selecting the right RF antenna
August 7, 2018
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Security and surveillance: Two sides of the coin in smart homes
By Martin Keenan   -   July 9, 2018
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Future proofing lighting systems with Bluetooth
By Alessandro Mastellari   -   May 9, 2018
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Optimising battery designs with supercapacitors
By Tim Parker   -   April 30, 2018
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
From enabled to proactive: The evolution of home automation
March 29, 2018
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
Man controlling home devices via his watch
Let your home do the work so you don't have to
By Martin Keenan   -   March 29, 2018
Today, we need to interact with connected products in the home deliberately. But it does not have to stay this way.
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Adapting PIR sensor technology to new applications
By Martin Keenan   -   February 7, 2018
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
EV charging points set to rapidly increase in numbers
By Marco Enge   -   January 18, 2018
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Protecting outdoor electronics against vandals
By Jerry Moss   -   December 18, 2017
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
RF When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Advances and trends in RF connection
By Marco Enge   -   October 19, 2017
When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
How wireless power transfer can help make the world’s lithium go further
By Martin Keenan   -   September 19, 2017
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
State-of-the-art wireless modules save time, space and money
By Martin Keenan   -   September 12, 2017
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
Automotive telematics become mandatory with eCall
By Alan Jermyn   -   August 1, 2017
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Datacentre racks
Chip-to-chip at the speed of light
By Marco Enge   -   March 31, 2017
As data centres and data farms continue to expand and grow, better solutions are required for system architectures that allow faster communication and more efficient operation.
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Hybrid capacitors combine technologies to get the best of both worlds
By Martin Keenan   -   March 15, 2017
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
Understanding ESR in electrolytic capacitors
By Adam Chidley   -   March 1, 2017
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
Design considerations for powering remote bluetooth beacons
By Tim Parker   -   February 9, 2017
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
As LED luminaires have continued to develop in complexity and range and the number of different fixtures on the market has increased, lighting designers have begun to demand more flexibility from their driver hardware.
Programmable drivers add flexibility to LED lighting
By Don Schriek   -   December 8, 2016
As LED luminaires have continued to develop in complexity and range and the number of different fixtures on the market has increased, lighting designers have begun to demand more flexibility from their driver hardware.
As one of the world’s leading manufacturers of wireless modules for smartphones, including supplying some of the very biggest names in the market, Murata knows a thing or two about wireless technologies, and also about manufacturing modules.
Designing for LoRaWAN - Murata wireless modules
By Martin Keenan   -   December 1, 2016
As one of the world’s leading manufacturers of wireless modules for smartphones, including supplying some of the very biggest names in the market, Murata knows a thing or two about wireless technologies, and also about manufacturing modules.
Bluetooth Beacons and NFC (Near Field Communication) are often mentioned in the same breath, but in terms of technology and applications, they are not really that similar.
NFC vs. Bluetooth beacons: More different than similar
By Martin Keenan   -   August 12, 2016
Bluetooth Beacons and NFC (Near Field Communication) are often mentioned in the same breath, but in terms of technology and applications, they are not really that similar.
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Ethernet magnetics – Discrete or integrated?
By Adam Chidley   -   July 29, 2016
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Selecting fibre optic cables
By Marco Enge   -   July 12, 2016
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Calculating LED heatsinks
By Giovanna Monari   -   May 22, 2016
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
The internet of medical things (IoMT) bringing better healthcare for all
By Martin Keenan   -   April 8, 2016
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
‘Wet’ aluminium and polymer aluminium capacitors – what’s the difference?
By Ekaterina Rachel   -   April 1, 2016
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Design trends: Batteries for IoT
By Tim Parker   -   March 11, 2016
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
Modern electromechanical relays meet today’s reliability demands
By Giovanna Monari   -   February 2, 2016
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Circuit protection is vital for long lifetimes in LED lighting
By Adam Chidley   -   January 7, 2016
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
Supercapacitors: Making transport more efficient
By Adam Chidley   -   September 7, 2015
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The unstoppable rise of polymer capacitors
By Ekaterina Rachel   -   August 10, 2015
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Understanding micro switches and hysteresis
By Giovanna Monari   -   June 12, 2015
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Fans have few fans, but perhaps they should?
By Mathias Goebel   -   May 28, 2015
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
What’s super about supercapacitors?
By Adam Chidley   -   May 18, 2015
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality.
How sensitivity to our environment is creating a growing market for air quality sensors
By Giovanna Monari   -   April 2, 2015
A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality.
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.
LED thermal management: Is it just me or is it getting hot in here?
By Giovanna Monari   -   March 19, 2015
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.

Multi-Standard Mesh Networking

Display portlet menu
Related Events