MOSFET Relays: Key Components In The Densification And Efficiency Of Electronics | Engineers' Insight | Avnet Abacus

Display portlet menu

MOSFET Relays: Key Components In The Densification And Efficiency Of Electronics | Engineers' Insight | Avnet Abacus

Display portlet menu

MOSFET relays: Key components in the densification and efficiency of electronics

Solar panels on a solar farm at sunrise


Traditional electromagnetic relays, (EMRs), are still popular choices for certain applications, particularly where high-power switching is required. But the characteristics of solid-state relays (SSRs), particularly MOSFET types, mean they are being employed in a growing range of applications. With the exponential growth of the IoT and the arrival of 5G networks driving a trend towards more powerful devices with shrinking form factors, engineers must fit more functionality into less space and find ways of improving switching speeds and power efficiencies. Certain key components in the modern IT infrastructure such as DC-DC converters and switching power supplies present specific design challenges which the characteristics of MOSFET relays can help to address. We look more closely at the MOSFET relay to understand how its characteristics are well suited to a number of key applications.
 

The MOSFET relay: A circuit rather than a switch

MOSFETs are actually electronic circuits, rather than relays, comprising an LED on the input side and a photodiode dome array (PDA), control circuit and FET block on the output side (Figure 1).

Figure 1: MOSFET block diagram

Within the MOSFET relay, the input driver circuit (1) causes current to flow through the LED, turning it on, and the light from the LED (2) is then converted to voltage by the PDA. (3) The PDA output voltage drives the MOSFET output block via a control circuit and the output block, which contains a double MOSFET, allows both AC and DC loads to pass in either direction.

With no moving parts, (unlike EMRs), MOSFET relays can withstand physical shock and vibration and will perform indefinitely when properly used, operating silently with very little electrical interference. The devices can handle a wide range of input voltages, consuming little power and there is no arcing during operation, making them suitable for hazardous environments. The inherent design of the MOSFET relay minimises surge currents and enables switching of both AC and DC signals. As well as their low power consumption, MOSFET relays are considerably smaller than their EMR counterparts, using less space on the PCB.
 

Characteristic Implication
Low output capacitance Improved switching times and isolation characteristics for high frequency load signals
Low on-resistance Reduced power dissipation when switching high currents and increased switching speeds
Physical isolation (galvanic separation) Physical isolation between the relay’s input and output or between different output channels enhances precision by minimising noise. Optically isolated relays offer a physical separation of input and output, with minimal leakage and isolation voltages as high as 5,000 volts AC.
High linearity MOSFET relays have a straight-line relationship between load current and load voltage, almost as good as EMR, ensuring no signal distortion. This characteristic also enables MOSFET relays to switch analogue and low-level signals.
Reliability With no moving parts, MOSFET relays have excellent an excellent failures in time (FIT) rate and are resistant to shock and vibration. MOSFET relays also eliminate the buzzing that can affect electromechanical relays driven by PWM and other methods intended to conserve input power.
Low operating cost Although higher-priced than EMR equivalents, their longer lifecycles and lower power consumption lead to lower overall operating costs for MOSFET relays.
Space saving MOSFET relays are considerably smaller than their EMR equivalents, offering up to a 95% space saving on the PCB.

Table 1: Summary of MOSFET relay characteristics
 

Typical applications for MOSFET relays

MOSFET relays are ideal for a wide range of applications, including automated test equipment, (ATE), medical equipment, security equipment, amusement equipment, factory automation, telecommunications, energy-related equipment and many more. The tables below provide an illustrative overview of how the characteristics of Omron’s MOSFET relay family benefit the design of a selection of applications, and the rest of this section examines a subset of these applications in more detail.

Security equipment

Smoke detectors, home security panels, PIR, video intercom systems
Function Features Recommended products
Status output
Signal output
General purpose G3VM-61VY3
G3VM-351VY
Ultrasensitive G3VM-61G2
1b (SPST-NC) G3VM-63G
G3VM-353G
Switching power supply of small solenoid valve, small motor external output High current G3VM-61VR
G3VM-61CR1/FR1
G3VM-201CR/FR
G3VM-601CR/FR
High dielectric strength G3VM-61AY1/DY1
G3VM-351AY1/DY1

Communication equipment 

Modems, fax machines, network devices, PNX transfer devices
Function Features Recommended products
Short-circuit line switching General purpose G3VM-61VY3
G3VM-351VY
Line switching 1b (SPST-NC) G3VM-63G
G3VM-353G

Entertainment equipment 

Currency sensing modules, coin dispensers, information systems
Function Features Recommended products
Status output
Signal output
General purpose G3VM-61VY3
G3VM-351VY
1b (SPST-NC) G3VM-63G
G3VM-353G

 

Automatic test equipment (ATE)

Semiconductor devices continue to become more complex and ever faster, challenging the designers of automatic test and measurement technology, who must incorporate higher numbers of test channels into their equipment in order to meet market demands for reduced testing time and improved efficiency. The low capacitance of MOSFET relays improves switching times and isolation characteristics for high frequency load signals. Their low on-resistance reduces power dissipation when switching high currents and increases switching speeds to improve measurement precision. Offering physical separation of input and output with minimal leakage, MOSFET relays also enhance measurement precision by reducing noise and their high linearity also contributes to measurement accuracy.

Function Features Recommended products
Switching test signal Low C x R G3VM-21UR1/UR10/UR11
G3VM-41UR10/UR11/UR12
G3VM-41QR10
G3VM-51UR
G3VM-61QR
Small and high-load -voltage G3VM-61UR1
High current G3VM-31QR
Switching power supply High current G3VM-31QR
G3VM-61QR2
G3VM-101QR1

 

Factory/industrial equipment

The Industry 4.0 smart factory leverages IoT technology and increased levels of automation to achieve cost-effective, flexible production capabilities. The factory environment is typically hostile to electronic equipment, however, and the high tolerance to physical shock and EMI of MOSFET relays make them ideal for the switching and protection of small motors, power supplies and control devices, with load currents up to 10 amps.

Function Features Recommended products
Status output
Signal output
General purporse G3VM-61VY3
G3VM-61A1/D1
G3VM-351VY
G3VM-351A/D
Switching power supply of small solenoid valve, small motor external output High current G3VM-61VR
G3VM-61CR1/FR1
G3VM-201CR/FR
G3VM-601CR/FR
High dielectric strength G3VM-61AY1/DY1
G3VM-351AY1/DY1

 

Energy-related equipment

Efficiency and densification are two important mega-trends within electronics, not least within the design of switching power supplies. The small form factors of MOSFET relays enable designers to reduce space on the PCB, their reduced output capacitance supports the high-speed switching requirements of modern power supply designs and their lower on-resistance contributes to cost savings through simpler heat management. Also, along with their low-power consumption, the improved noise performance of MOSFET relays contributes to the reduction of electromagnetic noise emission in high-end power supplies for equipment such as LCD TVs, LED lighting, medical power supplies and notebook power adapters.
 

Function Features Recommended products
External communications
Charge voltage monitoring
High dielectric strength G3VM-61AY1/DY1
G3VM-351AY1/DY1
G3VM-601AY1/DY1
General purpose G3VM-61VY3
G3VM-351VY
Storage battery charging High current G3VM-61CR1/FR1

 

Omron MOSFET relay product line

A global leader in the fields of industrial automation, electronic component industries and healthcare, Omron Corporation provides a variety of products and services, including a range of MOSFETs that set the benchmark for Solid State Relays. Manufactured using the latest advances in automated production and including a variety of improved construction technologies within the areas of LED, PDA and FET chips, Omron’s G3VM MOSFET relay family includes up to 200 devices that handle a wide range of voltages and currents (Figure 3). Options include current limiting, high-dielectric-voltage withstand, normally open and normally closed contact forms, and high-speed switching.

The key features of Omron’s G3VM MOSFET relay family include:

  • A wide range of packages: DIP, SOP, SSOP, USOP, VSON, and S-VSON
  • S-VSON package is the smallest in the industry: 2 x 1.45 x 1.65 mm
  • Single- and dual-contact models available with both NO and NC contacts
  • ON-resistance as low as 5 mΩ (typical)
  • OFF-state capacitance as low as 0.3 pF (typical)
  • Trigger LED forward currents as low as 0.2 mA
  • Switching times down to 0.2 ms
  • Models including current limiting functions also available
  • 100,000 hours of continuous operation
  • Dielectric strength up to 5,000 Vac for 1 second
  • Models switching up to 10 A* in such a small package
     

Reference table for Omron's relay rangeFigure 3: Omron's MOSFET relay product range

Conclusion

In a world where densification and efficiency are driving the design of electronic devices and systems, the characteristics of MOSFET relays are responsible for their incorporation in a growing range of applications. As a global leader in electronic components, Omron’s G3VM MOSFET relay range sets the standard. To find out more about the range, download datasheets, and purchase pilot samples click below. Alternatively, if you have specific requirements and would like to discuss your design in detail, click the Ask an Expert button to get in touch with one of our technical specialists in your local language.

Want more like this? Sign up to our newsletters

MOSFET Relays: Key Components In The Densification And Efficiency Of Electronics | Engineers' Insight | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Webinar

Circuit design with MOSFET relays

Watch Omron’s MOSFET webinar with Element 14.

MOSFET Relays: Key Components In The Densification And Efficiency Of Electronics | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Articles
A photo of various antennas laid out on a white background
4 keys to selecting antennas for small IoT devices
November 19, 2019
Wireless connectivity is a critical enabler for many IoT applications. While a wireless module can simplify the RF subsystem design, a working system requires careful selection of an antenna as well.
Tesla plugged into charging station
Switching high voltages and currents with PCB-mounted relays
By Martin Keenan   -   November 8, 2019
The growing demand for safe, robust and energy-efficient ways to switch relatively large amounts of power means that relays have an important role to play in a wide range of modern applications.
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
These 8 charts will challenge your perspective on the Industrial IoT
October 1, 2019
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
Maximise your IIoT installation success by choosing the right sensors
July 19, 2019
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.
How to choose the right DC-DC converter for HV gate driver applications
By Philip Lechner   -   January 31, 2019
Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.
Rapidly increasing market demand and the rationalisation of product offerings from Li-ion cell manufacturers are impacting the choices available to design engineers.
Strategies to combat volatility in the lithium-ion battery market
By Tim Parker   -   November 22, 2018
Rapidly increasing market demand and the rationalisation of product offerings from Li-ion cell manufacturers are impacting the choices available to design engineers. Here Tim Parker discusses the background to these dynamics and how engineers can suc
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
DC-DC power conversion challenges in transportation applications
By Andrew Hutton   -   November 22, 2018
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
When configurable power supplies are the best solution
By Hector Garcia   -   November 20, 2018
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
How wireless power transfer can help make the world’s lithium go further
By Martin Keenan   -   September 19, 2017
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
State-of-the-art wireless modules save time, space and money
By Martin Keenan   -   September 12, 2017
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Hybrid capacitors combine technologies to get the best of both worlds
By Martin Keenan   -   March 15, 2017
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.

MOSFET Relays: Key Components In The Densification And Efficiency Of Electronics | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Events