An Introduction to EV Charging Infrastructure Design | Engineers' Insight | Avnet Abacus

Display portlet menu

An Introduction to EV Charging Infrastructure Design | Engineers' Insight | Avnet Abacus

Display portlet menu

An introduction to EV charging infrastructure design

An electric vehicle charging cable being plugged into a charging station

The rate at which electric vehicles (EV) can be charged is becoming a key differentiator in this rapidly developing market, for a very straightforward reason: charging an EV’s battery is currently a lot slower than refilling a tank with petrol to go the same distance.

Take a generic EV with a battery capacity of 60kWh. Charging this battery from zero to 100%, using a cable plugged in to a standard UK 240V, 13A socket, will take about 20 hours. This isn’t practical for a daily driver, much less for a long-distance traveller.

In practice, most EV owners rely on dedicated chargers, often wired in at home to higher-current ring mains. UK energy supplier E-On, for example, will wire a 7.4kW wall-mounted charger, with either a tethered charging cable or a universal socket for a charging cable, into a 32A ring main. With this charger, our generic 60kWh EV can be charged in more like eight and a half hours.
 

A hierarchy of charging

The rapid growth of the EV market has led to a proliferation of connection and charging strategies, charger designs and charging networks.

Slow chargers are typically rated at 3kW, and are mostly used in homes, ideally through a dedicated wall-box. They’re not really suitable for public use because they charge too slowly.

Fast chargers are found in public places, such as car parks and shopping centres, and may charge at rates of 7kW or 22kW. A 22kW charger could charge our generic 60kWh EV from zero to a full charge in around two and half to three hours.

Rapid chargers often charge using DC, handling the rectification of the AC supply within the charger rather than relying on the EV’s onboard rectifier. Rapid DC chargers commonly provide up to 50kW of power, while rapid AC units are commonly rated up to 43kW. At a 50kW charging rate, our generic EV battery would be recharged in just over an hour.

 
Figure 1: The Lotus Evija will charge at rates up to 800kW (Source: Lotus)

Tesla goes one better with its current Superchargers, which charge at 120kW through a proprietary connector. Tesla has also announced its V3 250kW supercharger, which it claims add 180 miles of range to a Tesla Model 3 with the long-range battery option in just 15 minutes.

At the top end of the EV scale, Lotus has just announced its Evija EV ‘hypercar’. The battery in this vehicle has been designed to accept charge at up to 800kW, a greater rate than commercially available chargers can yet provide. Once 800KW chargers are available, Lotus says the Evija’s battery could be fully recharged in nine minutes. Using more widely available 350kW chargers, the Evija will take 18 minutes to charge to 100%.

They are only going to build 130 Evijas, so most of us needn’t worry about finding 800kW chargers any time soon, but, as with Formula 1 technology development, this Lotus hypercar is a pathfinder for future mainstream adoption.
 

Getting connected

Along with a hierarchy of charging options, all of which affect an EV’s ‘miles per hour’ there is also a variety of charging connector options, each of which is (mainly) incompatible with the others.

Figure 2: Connector options for EVs

The single-phase AC Type 1 connector, common in Asia, supports charging at up to 7.4kW. Type 2 plugs support three-phase AC charging, at up to 22kW in private settings, and up to 43kW at public charging stations. CCS plugs add two more contacts to a Type 2 plug for fast charging, enabling AC and DC charging at up to 170kW. The CHAdeMO connector allows for charging powers up to 50kW. Tesla uses a modified version of the Type 2 Mennekes plug for its proprietary fast-charging approach. In China, the GB/T fast-charging connector is becoming popular.

These are deployed as follows, at least in the UK. Slow charging is carried out at 3kW using either a standard 3pin plug, a Type or Type 2 connector, or even the ‘commando’ connectors used on caravans. Fast charging, at between 7 and 22kW AC, is done using Type 1 and 2 connectors. Rapid charging is done at 50kW DC using the CHAdeMo or CCS connectors, at 43kW AC using the Type 2 connector, and at 120kW DC using the Tesla Type 2 connector variant. Many vehicles have more than one socket, to enable access to both slow and fast charging stations.
 

Charging networks

The uptake of EVs has led to the rapid development of competing charging networks.

Open Charge Map, a global public registry of charging locations, lists 151,060 charging stations at 74,380 locations, including above the Arctic Circle at the airport on Svalbard Island, and at Tokanui on the southern tip of New Zealand’s southern island.

Some companies are installing charging points as a standalone offering, while others are doing so to diversify their businesses. It makes sense that oil companies BP and Shell would install chargers to keep up with their evolving customer base, but in Germany utility company Telekom, the former state telecoms company, is entering the market by piggybacking a charging network on its communications infrastructure.

The company has installed public charging stations in Bonn and Darmstadt, each offering two vehicles charging at 11kW over a type 2 plug. In Bonn, Telekom has gone a step further with its first 150kW charging station, which will add 100km to an EV’s range in ten minutes. The company plans to introduce 500 rapid chargers in the next three years.

Eurotunnel is also leveraging its infrastructure to support EV driving by installing chargers at both its terminals, with charging for Teslas as well as for any other EV or hybrid that has a CHAdeMO or Type 2 interface.

Car makers are getting in on the act, too. For example, IONITY is a joint venture between BMW, Daimler, Ford, and Volkswagen with its Audi and Porsche brands to build a high-power (350kW) charging network along Europe’s major highways. Its network already reaches from Sweden to northern Spain, with more chargers due to be installed soon.

Energy company E.ON is cooperating with Danish mobility service provider CLEVER to build a similar north-south, ultra-fast charging network in Europe.

The plan is to install several hundred 150kW charging locations, at distances of 120 to 180km apart along the major motorways. An upgrade to 350kW should follow as technology allows.

E.ON already operates 1,200 public charging points and 39 fast chargers in Denmark. CLEVER has been developing a fast-charging network in Denmark, Sweden and Northern Germany since 2009. The joint initiative is co-financed by the Connecting Europe facility of the European Union.

Of course, not all networks charge all EVs in the same way or are equally accessible to all.

Zap-Map, an online platform for all things related to EVs and the supporting charging infrastructure, collates statistics on the growth of the UK’s charging infrastructure. According to the site, as of 26 July 2019, the UK has 9,167 public charging points, with a total of 14,571 devices and 24,768 connectors across those sites. The site has added details of 522 new devices and 857 new connectors in the past 30 days.

Zap-Map stats also show that there are 1605 public rapid charging points in the UK, hosting 2,338 devices and a total of 5,412 rapid connectors. 232 new rapid connectors have been added to Zap-Map’s database in the past 30 days.

EV charging has prompted the development of multiple charging networks, each founded on a slightly different business model. Here are a few examples.

Polar, operated by BP Chargemaster, is the UK’s public charging network It offers both subscription and pay-as-you-go services, accessed either by an RFID card or via a smartphone app.

Pod Point operates the Pod Point network of mainly fast and rapid chargers, many of which are free to use although some have a pay-as-you-go charge.

Charge Your Car is the largest pay-as-you-go network in the UK. It operates, but doesn’t own, a network of charge points across the UK, providing back-office services to the charging units’ owners. Its customers include regional providers, such as Source West, and ChargePlace Scotland, which is backed by the Scottish government.

Zap-Map itself has set up Zap-Home and Zap-Work, peer-to-peer charging networks through which home or business owners can offer registered users access to their chargers under conditions which they set themselves. Payments, if there are any, happen over PayPal.
 

Charger design

The dynamism of the EV marketplace is demanding the development of a wide variety of charging options, usually predicated upon where they will be used.

Home charging solutions can be as simple as using a standard EVSE (Electric Vehicle Supply Equipment) charging cable to plug into a mains socket, or as complex as installing a wall-mounted charger. The design challenge here is to develop a safe, easy to install, charger suitable for production in relatively large volumes.

Workplaces are beginning to install EV charging, to help make EVs viable for staff with long commutes, as well as for visiting customers. The design challenge here is to produce a flexible charging system that can be easily installed in multiple units on a site, perhaps with centralised management, and sophisticated access controls to enable, for example, guest usage.

Chargers for use in public venues must be robust, support fast and, ideally rapid charging rates, and adapt automatically to serve multiple different vehicle types and battery conditions. They often support multiple connections per charger (two is popular). They also need to enable access by customers from multiple public charging services that have developed reciprocal access arrangements to extend their geographical coverage. The design challenge here is to deliver large amounts of charging power in a way that is safe, robust and easy to use.
 

Connectivity options

Even what appear to be the simplest components need careful thought in the context of EV charging.

For example, ITT Cannon offers the ECIER EV charging outlet. It is an IEC (Type 2) EVSE rear-mount outlet that provides low contact resistance and a minimum of 10,000 mating cycles. It is available for single- and three-phase charging systems and has a current rating up to 63A. The outlet uses a canted coil spring to minimise mechanical stress, mis-alignment and power loss. Customisation options include a compression limiter, dust cap, spring cap, drain spout and locking devices.

For chargers with tethered cables, Aptiv produces connectors and pigtail cables with an emphasis on durability, weather sealing, CE, CQC, and UL markings, and compliance with multiple automotive standards including SAE J1772/IEC62196 Type I, IEC62196 Type II, and GB/T 20234.

TE Connectivity also makes charger cables for multiple regions and countries, for use in harsh environments. They are designed to mate more than 10,000 times, thanks to ultrasound welding for sealing and robustness. Safety features include ground monitoring, to detect residual currents, mis-wiring detection, over- and under-voltage management, over-current management to protect against shorts, and overheating detection to monitor the temperature in the charging unit as well as the infrastructure plug.

TE Connectivity is researching the implications of the continuous high current flows, of up to 500A, involved in charging a vehicle at 350kW. The aim of charging at this rate is to make it possible to increase a vehicle’s range by 300km in ten minutes, but this sixteen-fold increase in charging rate brings with it a 256-fold increase in heat dissipation.

Designers are responding by considering using much thicker (and therefore heavier and more costly) cables, or increasing the working voltage of battery packs to 800V. Designers will also have to adjust the assumptions they use to specify components, to take into account the sustained high currents created by high-power charging as compared to the intermittent high current draws of driving.

Figure 3: The high-current path from charger to EV battery pack (Source: TE Connectivity)

This, in turn, will drive the choice of components and connectivity options within the charger’s internal circuitry. TE Connectivity argues that designers need to take a systemic approach to thermal management in the high-voltage, high-current environment of EV chargers. Failing to properly manage the thermal dissipation of any component in the path from the charging infrastructure to the battery pack (see Figure 3) will undermine the efficacy of the whole system.

Amphenol has developed two related connector ranges that address this issue. The ePower connectors are designed for use in hybrid, EV, and utility truck electrical systems, operating at 800V DC to 1000V DC with a 200A to 500A rating. The connectors use patented RADSOK technology to reduce interconnect resistance to enable higher currents with lower temperature rises. The connectors are also designed to save space, so that one 400A ePower connector can replace three conventional connectors.

The related ePower-Lite range is a plastic power connector for use in hybrid EVs, again using the RADSOK technology to reduce connection resistance. The compact, plastic shell is light, and the connector can be installed and repaired in the field.

These are just some examples of the way in which the enabling technology for EVs is evolving. It’s clear that although a lot has already been done, there’s plenty of work left to do to boost the ‘miles per hour’ of EVs. Visit our automotive page to explore our range of solutions for EV charging systems, or if you would like to speak to one of our technical specialists about your design, click the Ask an Expert button to get in touch in your local language.

An Introduction to EV Charging Infrastructure Design | Engineers' Insight | Avnet Abacus

Display portlet menu

An Introduction to EV Charging Infrastructure Design | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Articles
Automation manufacture Industry 4.0
Evolution before revolution: the origins of Industry 4.0
May 27, 2020
We’ve come a long way from the days of Henry Ford famously telling customers that they could have the Model T car painted any colour ‘so long as it was black’ – a quote which reflected the compromise of having to put efficiency before choice.
Product
The evolution of cellular networks
By Martin Keenan   -   April 29, 2020
Since the first 5G services were launched in the USA by Verizon and AT&T, 5G networks have been rolled out in a further 17 countries with South Korea, the United Kingdom, Germany, and the United States leading the charge and China catching up fast.
Abstract image of an electronic circuit
How SiC and GaN technology is affecting passive component development
June 19, 2020
To keep up with the semiconductor process innovations, SiC and GaN present some unique challenges to the essential passive components used in power conversion and motor drive circuits.
Satellite in action around the Earth
The future is 5G
By Adam Chidley   -   April 29, 2020
'The explosive growth of the IoT shows no signs of abating, with Gartner forecasting 20.8 billion connected “things” by 2020, and IHS Markit predicting that this number will rise to 125 billion by 2030.'
A technical specialist on solar panels
Extending battery lifetime in wireless applications using supercapacitors
By Martin Keenan   -   April 20, 2020
This article describes how supercapacitors can be deployed in conjunction with batteries to extend their operational life and reduce maintenance and replacement costs.
Engineer using an oscilloscope to test a circuit
Selecting relays for test and measurement equipment
By Shlomo Avital   -   March 30, 2020
One of the key challenges with developing test and measurement equipment is to ensure that the signal that gets measured is the same as the signal that you want to measure. It sounds obvious, but multiple factors in the path from the test point to the me...
Inside of a connected car depicting
V2X: The future of vehicle communications
By Martin Keenan   -   December 10, 2019
Vehicles are about to become a lot more communicative: with other road users, with the infrastructure they pass on their journeys, with cloud-based services, and even with the energy grid. This communication should make vehicles more economical to operate...
Tesla plugged into charging station
Switching high voltages and currents with PCB-mounted relays
By Martin Keenan   -   November 8, 2019
The growing demand for safe, robust and energy-efficient ways to switch relatively large amounts of power means that relays have an important role to play in a wide range of modern applications.
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
The complex electronic architectures of  hybrid and electric vehicles have required engineers to rethink power requirements. Here's why 48V DC systems are key to modern automotive systems, and some considerations on powertrain component selection.
The shift to 48V in automotive systems: What you need to know
October 18, 2019
The complex electronic architectures of hybrid and electric vehicles have required engineers to rethink power requirements. Here's why 48V DC systems are key to modern automotive systems, and some considerations on powertrain component selection.
While connectors are not the most interesting components in automotive systems, they can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
4 factors steering connector choices in today's automotive applications
September 16, 2019
Connectors are critical components in any automotive systems, and their selection can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
A quick guide to multi-standard mesh networking
By Alessandro Mastellari   -   April 11, 2019
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
A quick guide to powering smart objects with kinetic energy harvesting
By Alessandro Mastellari   -   January 22, 2019
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Design trends: Automotive passives
By Martin Keenan   -   November 29, 2018
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
DC-DC power conversion challenges in transportation applications
By Andrew Hutton   -   November 22, 2018
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
Key design considerations for selecting the right RF antenna
August 7, 2018
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Security and surveillance: Two sides of the coin in smart homes
By Martin Keenan   -   July 9, 2018
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Future proofing lighting systems with Bluetooth
By Alessandro Mastellari   -   May 9, 2018
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Optimising battery designs with supercapacitors
By Tim Parker   -   April 30, 2018
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Man controlling home devices via his watch
Let your home do the work so you don't have to
By Martin Keenan   -   March 29, 2018
Today, we need to interact with connected products in the home deliberately. But it does not have to stay this way.
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
EV charging points set to rapidly increase in numbers
By Marco Enge   -   January 18, 2018
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Protecting outdoor electronics against vandals
By Jerry Moss   -   December 18, 2017
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
RF When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Advances and trends in RF connection
By Marco Enge   -   October 19, 2017
When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
How wireless power transfer can help make the world’s lithium go further
By Martin Keenan   -   September 19, 2017
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
Automotive telematics become mandatory with eCall
By Alan Jermyn   -   August 1, 2017
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Meeting regulatory requirements for mission-critical and non-mission-critical rolling stock power supplies
By Philip Lechner   -   June 13, 2017
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Datacentre racks
Chip-to-chip at the speed of light
By Marco Enge   -   March 31, 2017
As data centres and data farms continue to expand and grow, better solutions are required for system architectures that allow faster communication and more efficient operation.
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Hybrid capacitors combine technologies to get the best of both worlds
By Martin Keenan   -   March 15, 2017
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
Understanding ESR in electrolytic capacitors
By Adam Chidley   -   March 1, 2017
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Ethernet magnetics – Discrete or integrated?
By Adam Chidley   -   July 29, 2016
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Selecting fibre optic cables
By Marco Enge   -   July 12, 2016
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Calculating LED heatsinks
By Giovanna Monari   -   May 22, 2016
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
‘Wet’ aluminium and polymer aluminium capacitors – what’s the difference?
By Ekaterina Rachel   -   April 1, 2016
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
Modern electromechanical relays meet today’s reliability demands
By Giovanna Monari   -   February 2, 2016
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Circuit protection is vital for long lifetimes in LED lighting
By Adam Chidley   -   January 7, 2016
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
Supercapacitors: Making transport more efficient
By Adam Chidley   -   September 7, 2015
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The unstoppable rise of polymer capacitors
By Ekaterina Rachel   -   August 10, 2015
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Understanding micro switches and hysteresis
By Giovanna Monari   -   June 12, 2015
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Fans have few fans, but perhaps they should?
By Mathias Goebel   -   May 28, 2015
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
What’s super about supercapacitors?
By Adam Chidley   -   May 18, 2015
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.
LED thermal management: Is it just me or is it getting hot in here?
By Giovanna Monari   -   March 19, 2015
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.

An Introduction to EV Charging Infrastructure Design | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Events