Supercapacitor And Li-Ion Technology Combining | Avnet Abacus

Display portlet menu

Supercapacitor And Li-Ion Technology Combining | Avnet Abacus

Display portlet menu

Hybrid capacitors combine technologies to get the best of both worlds

Martin Keenan Photo

Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.

Supercapacitors are commonly used wherever a quick energy boost is needed, as an alternative to a rechargeable battery. The most prevalent type of supercapacitors, EDLCs (electrical double layer capacitors), provide thousands or tens of thousands of times the capacitance of normal capacitors while their energy density makes them 10 times smaller than batteries (more here about how EDLCs work in detail). However, while EDLCs offer high capacitance, excellent power density and impressive efficiency, there are a few inherent properties which aren’t as desirable for some applications.

For example, most devices exhibit a characteristic called self-discharge, which means that if not discharged after a short time, the stored energy will leak away. The effect is particularly pronounced at high temperatures. Both leakage current and ESR (equivalent series resistance) can also exclude EDLCs from certain applications. The alternative, a secondary lithium ion (Li-ion) battery, offers higher energy density with reduced self-discharge, but they effectively wear out after a number of charge/discharge cycles. They also suffer from safety-related concerns such as thermal runaway, which can be catastrophic.

There is another device type on the market which combines the best features of EDLCs and Li-ion batteries. Called Li-ion capacitors, or hybrid capacitors, they are effectively a combination of the two technologies. While EDLCs hold energy using electrostatic charge, and Li-ion batteries use an electrochemical method, Li-ion capacitors use one electrostatic electrode and one electrochemical. The result is a device with better energy density than an EDLC, but without the self-discharge characteristic, and higher durability (more charge-discharge cycles) than a Li-ion battery, without the potential for dangerous thermal runaway.

Inside a Li-ion capacitor (pictured left), the positive electrode is made of activated carbon. This is immersed in a liquid electrolyte (similar to the Li-ion salt solution used in batteries) together with the negative electrode, made of a carbon-based material doped with  lithium ions. A separator prevents direct electrical of a carbon-based material doped with lithium ions. A separator prevents direct electrical contact. Pre-a carbon-based material doped with lithium ions. A separator prevents direct electrical contact. Pre-doping the negative electrode with lithium ions reduces its electrical potential, meaning a higher output voltage can be obtained without a high potential at the positive electrode, up to around 3.8V. Since the energy density is proportional to the squareput voltage can be obtained without a high potential at the positive electrode, up to around 3.8V. Since the energy density is proportional to the square of this voltage, Li-ion capacitors are several times more energy dense than EDLCs, with a similar power density. What this means is the same amount of energy can be stored in a much more compact Li-ion capacitor than the equivalent EDLC, contributing to keeping device size small. The pre-doping also helps to stabilise the electrode’s potential, meaning there is very little self-discharge (see graph to the left). 

Compared to a Li-ion battery, in which the ions are inserted or extracted (intercalated or deintercalated) into the carbon lattice, ions in the Li-ion capacitor are simply adsorbed or desorbed on the electrode surface, there is no crystalline change taking place. This gives Li-ion capacitors a big advantage over batteries in terms of the number of charge/discharge cycles they can withstand, similar to the longevity of EDLCs. Li-ion capacitors also do not contain oxygen or oxides, so they are not prone to thermal runaway conditions. This makes them a safer alternative to Li-ion batteries. A full comparison table between the technologies is shown below. 


Comparing the properties of EDLCs, Li-ion capacitors and Li-ion batteries (LIBs)




 

 

As an example of some real-world devices, Avnet Abacus carries Li-ion capacitor parts from Taiyo Yuden between 40 and 270F (17.77 to 120 mAh) with an ESR as low as 0.05 Ω (right). These come in cylindrical metal casings and the smallest in the series is 35mm x 12.5mm. The operating temperature range is -25 to +70°C, but this can be extended to +85°C by reducing the operating voltage from 3.8 to 3.5V. A range of large capacitance devices is also under development – expected to cover the range 500 to 1000F (222 to 1420 mAh).

The different properties of EDLCs, Li-ion batteries and Li-ion capacitors suits each technology to various different applications. Li-ion capacitors are ideal for applications that demand high energy density, high power density, low leakage, longevity, durability and safety, as well as anywhere where the operating temperature is too high for efficient operation of EDLCs. This can include backup power sources for memory and other ICs, auxiliary power devices for energy-saving purposes (such as rapid drum heating in copiers and on start-up for projectors) and automotive electronics which are subject to harsh temperatures.

A key new application area for Li-ion capacitors is power supplies for energy harvesting devices, as they are quickly rechargeable, lightweight and don’t self-discharge. They can store the energy generated and produce it quickly when, say, wireless transmission is needed. Since they don’t wear out, the maintenance cost for changing coin cell batteries is eliminated. We expect to see many new types of small energy-harvesting applications enabled as a direct result of this exciting technology.  

If you are interested in Li-ion capacitor technology and would like to discuss your latest design requirements with one of our regional product specialists, click here to get in touch.

Want more like this? Sign up for our newsletters

About Author

Martin Keenan Photo
Martin Keenan

As Technical Director, Martin is responsible for technical marketing strategy across IP&E, power and...

Supercapacitor And Li-Ion Technology Combining | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Supercapacitor And Li-Ion Technology Combining | Avnet Abacus

Display portlet menu
Related Articles
An electric vehicle charging cable being plugged into a charging station
An introduction to EV charging infrastructure design
February 7, 2020
With demand for faster charging of EV vehicles increasing, the design of charging stations and infrastructure becomes ever more important.
Inside of a connected car depicting
V2X: The future of vehicle communications
By Martin Keenan   -   December 10, 2019
Vehicles are about to become a lot more communicative: with other road users, with the infrastructure they pass on their journeys, with cloud-based services, and even with the energy grid. This communication should make vehicles more economical to operate...
Solar panels on a solar farm at sunrise
MOSFET relays: Key components in the densification and efficiency of electronics
November 27, 2019
Traditional electromagnetic relays, (EMRs), are still popular choices for certain applications, particularly where high-power switching is required, but increasingly, MOSFETs are being used in modern applications.
A photo of various antennas laid out on a white background
4 keys to selecting antennas for small IoT devices
November 19, 2019
Wireless connectivity is a critical enabler for many IoT applications. While a wireless module can simplify the RF subsystem design, a working system requires careful selection of an antenna as well.
Bigger is always better, isn’t it? That’s not necessarily the case when it comes to specifying a power supply.
AC-DC power supply design: how to specify capacity
January 15, 2020
AC-DC power supply design - how to pick an AC-DC power supply, and 80 PLUS Certification in context
Tesla plugged into charging station
Switching high voltages and currents with PCB-mounted relays
By Martin Keenan   -   November 8, 2019
The growing demand for safe, robust and energy-efficient ways to switch relatively large amounts of power means that relays have an important role to play in a wide range of modern applications.
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
These 8 charts will challenge your perspective on the Industrial IoT
October 1, 2019
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
While connectors are not the most interesting components in automotive systems, they can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
4 factors steering connector choices in today's automotive applications
September 16, 2019
While connectors are not the most interesting components in automotive systems, they can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
Maximise your IIoT installation success by choosing the right sensors
July 19, 2019
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
A quick guide to multi-standard mesh networking
By Alessandro Mastellari   -   April 11, 2019
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.
How to choose the right DC-DC converter for HV gate driver applications
By Philip Lechner   -   January 31, 2019
Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
A quick guide to powering smart objects with kinetic energy harvesting
By Alessandro Mastellari   -   January 22, 2019
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
Andy Hutton investigates the problems that LED flicker can cause in day-to-day life and the steps designers can take to prevent it in their lighting applications.
What is LED flicker - and how to prevent it
By Andrew Hutton   -   January 9, 2019
Andy Hutton investigates the problems that LED flicker can cause in day-to-day life and the steps designers can take to prevent it in their lighting applications.
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Design trends: Automotive passives
By Martin Keenan   -   November 29, 2018
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
ENEC (European Norms Electrical Certification) is the European hallmark for luminaires and related products and is used to demonstrate compliance with European safety standards. This certification system also includes LED drivers
Designing safe certified and efficient power solutions for LED lighting system
By Philip Lechner   -   November 22, 2018
ENEC (European Norms Electrical Certification) is the European hallmark for luminaires and related products and is used to demonstrate compliance with European safety standards. This certification system also includes LED drivers - the electronics th
Rapidly increasing market demand and the rationalisation of product offerings from Li-ion cell manufacturers are impacting the choices available to design engineers.
Strategies to combat volatility in the lithium-ion battery market
By Tim Parker   -   November 22, 2018
Rapidly increasing market demand and the rationalisation of product offerings from Li-ion cell manufacturers are impacting the choices available to design engineers. Here Tim Parker discusses the background to these dynamics and how engineers can suc
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
DC-DC power conversion challenges in transportation applications
By Andrew Hutton   -   November 22, 2018
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
When configurable power supplies are the best solution
By Hector Garcia   -   November 20, 2018
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
Key design considerations for selecting the right RF antenna
August 7, 2018
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Security and surveillance: Two sides of the coin in smart homes
By Martin Keenan   -   July 9, 2018
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Future proofing lighting systems with Bluetooth
By Alessandro Mastellari   -   May 9, 2018
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Optimising battery designs with supercapacitors
By Tim Parker   -   April 30, 2018
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Man controlling home devices via his watch
Let your home do the work so you don't have to
By Martin Keenan   -   March 29, 2018
Today, we need to interact with connected products in the home deliberately. But it does not have to stay this way.
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Adapting PIR sensor technology to new applications
By Martin Keenan   -   February 7, 2018
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
EV charging points set to rapidly increase in numbers
By Marco Enge   -   January 18, 2018
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Protecting outdoor electronics against vandals
By Jerry Moss   -   December 18, 2017
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
RF When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Advances and trends in RF connection
By Marco Enge   -   October 19, 2017
When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
How wireless power transfer can help make the world’s lithium go further
By Martin Keenan   -   September 19, 2017
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
The market for consumer robots aimed at learning and education is growing rapidly, but selecting the right battery can make or break a companion robot's design.
Consumer robot designs present a challenge for Li-ion batteries
By Tim Parker   -   September 18, 2017
The market for consumer robots aimed at learning and education is growing rapidly, but selecting the right battery can make or break a companion robot's design.
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
State-of-the-art wireless modules save time, space and money
By Martin Keenan   -   September 12, 2017
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
Automotive telematics become mandatory with eCall
By Alan Jermyn   -   August 1, 2017
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Meeting regulatory requirements for mission-critical and non-mission-critical rolling stock power supplies
By Philip Lechner   -   June 13, 2017
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Datacentre racks
Chip-to-chip at the speed of light
By Marco Enge   -   March 31, 2017
As data centres and data farms continue to expand and grow, better solutions are required for system architectures that allow faster communication and more efficient operation.
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
Understanding ESR in electrolytic capacitors
By Adam Chidley   -   March 1, 2017
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
Design considerations for powering remote bluetooth beacons
By Tim Parker   -   February 9, 2017
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
As LED luminaires have continued to develop in complexity and range and the number of different fixtures on the market has increased, lighting designers have begun to demand more flexibility from their driver hardware.
Programmable drivers add flexibility to LED lighting
By Don Schriek   -   December 8, 2016
As LED luminaires have continued to develop in complexity and range and the number of different fixtures on the market has increased, lighting designers have begun to demand more flexibility from their driver hardware.
As one of the world’s leading manufacturers of wireless modules for smartphones, including supplying some of the very biggest names in the market, Murata knows a thing or two about wireless technologies, and also about manufacturing modules.
Designing for LoRaWAN - Murata wireless modules
By Martin Keenan   -   December 1, 2016
As one of the world’s leading manufacturers of wireless modules for smartphones, including supplying some of the very biggest names in the market, Murata knows a thing or two about wireless technologies, and also about manufacturing modules.
If the feedback circuitry in a secondary-side regulated flyback converter could somehow be integrated into the switcher IC while maintaining isolation, the circuit would use fewer components and be smaller, simpler and cheaper overall.
Simplifying SMPS design with the right switching IC plus easy custom magnetics
By Philip Lechner   -   November 5, 2016
If the feedback circuitry in a secondary-side regulated flyback converter could somehow be integrated into the switcher IC while maintaining isolation, the circuit would use fewer components and be smaller, simpler and cheaper overall.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Bluetooth Beacons and NFC (Near Field Communication) are often mentioned in the same breath, but in terms of technology and applications, they are not really that similar.
NFC vs. Bluetooth beacons: More different than similar
By Martin Keenan   -   August 12, 2016
Bluetooth Beacons and NFC (Near Field Communication) are often mentioned in the same breath, but in terms of technology and applications, they are not really that similar.
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Ethernet magnetics – Discrete or integrated?
By Adam Chidley   -   July 29, 2016
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Selecting fibre optic cables
By Marco Enge   -   July 12, 2016
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Since the 1990s, the external power supply has become the target of a series of regulations that are gradually being tightened around the world.
The power regulations spiral
By Andrew Hutton   -   May 24, 2016
Since the 1990s, the external power supply has become the target of a series of regulations that are gradually being tightened around the world.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Calculating LED heatsinks
By Giovanna Monari   -   May 22, 2016
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Specifying medical power supplies can be particularly challenging because of the standards and jargon surrounding this application.
Deciphering datasheets for medical PSUs
By Philip Lechner   -   April 29, 2016
Specifying medical power supplies can be particularly challenging because of the standards and jargon surrounding this application.
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
The internet of medical things (IoMT) bringing better healthcare for all
By Martin Keenan   -   April 8, 2016
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
‘Wet’ aluminium and polymer aluminium capacitors – what’s the difference?
By Ekaterina Rachel   -   April 1, 2016
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Design trends: Batteries for IoT
By Tim Parker   -   March 11, 2016
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
Modern electromechanical relays meet today’s reliability demands
By Giovanna Monari   -   February 2, 2016
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Circuit protection is vital for long lifetimes in LED lighting
By Adam Chidley   -   January 7, 2016
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
Supercapacitors: Making transport more efficient
By Adam Chidley   -   September 7, 2015
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The unstoppable rise of polymer capacitors
By Ekaterina Rachel   -   August 10, 2015
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
Lithium batteries have been in the news again recently, unfortunately for all the wrong reasons.
How to impose a smoking ban on lithium batteries
By Tim Parker   -   July 9, 2015
Lithium batteries have been in the news again recently, unfortunately for all the wrong reasons.
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Understanding micro switches and hysteresis
By Giovanna Monari   -   June 12, 2015
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Fans have few fans, but perhaps they should?
By Mathias Goebel   -   May 28, 2015
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
What’s super about supercapacitors?
By Adam Chidley   -   May 18, 2015
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Keenly associated to the trend of greater computing power and complexity is a technology that is making a move into industrial from the communications field: that of advanced power system architectures.
Advanced power architectures move into industry
By Philip Lechner   -   April 20, 2015
Keenly associated to the trend of greater computing power and complexity is a technology that is making a move into industrial from the communications field: that of advanced power system architectures.
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.
LED thermal management: Is it just me or is it getting hot in here?
By Giovanna Monari   -   March 19, 2015
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.

Supercapacitor And Li-Ion Technology Combining | Avnet Abacus

Display portlet menu
Related Events
Embedded World 2020
Date: February 25, 2020
Location: Nuremburg, Germany