How to choose the right DC-DC converter for HV gate driver applications | Avnet Abacus

Display portlet menu

How to choose the right DC-DC converter for HV gate driver applications | Avnet Abacus

Display portlet menu

How to choose the right DC-DC converter for HV gate driver applications

Philip Lechner Photo

Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.

Bridge circuits using ‘high-side’ switches are common in applications from inverters to motor control (Figure 1, right). However, the high-side gate drive return is actually a switching node so the gate driver and its associated power rails are offset from ground by a high voltage, high frequency waveform with fast edges. While you can achieve this offset for the driver power rails with charge pumps, isolated DC-DC converters are often preferred and are actually necessary when safety isolation is required between control and power circuitry. Gate drive power can also be surprisingly high – 2W is typical for small systems but can be 10W+, especially when using large IGBTs. Power requirement scales directly with frequency so even newer technologies such as SiC and GaN with low gate charge need significant power when run at high speed.
 

Gate drive voltages are often bipolar and asymmetrical

The DC-DC has to be right for this application though – gates of IGBTs and MOSFETs of all technologies are often driven with asymmetric bipolar voltages. Even though data sheets might indicate that 0V is adequate for the OFF-drive, ‘Miller’ capacitance between gate and collector (drain) tends to inject charge opposing the gate drive so a negative drive ensures reliable switching. The same effect occurs with any emitter (source) inductance that is common to the gate drive loop: with high di/dt levels, a voltage transient is generated which again opposes gate drive. With packaged devices, this common inductance is inevitable and even a few nH causes volts of spikes with realistic rates of change of current. The bipolar gate drive voltage can be relatively uncritical for some devices such as Si-MOSFETs with typically +/-12V but SiC and GaN need to be much more exact with +6/-3V often recommended for GaN, for example.
 

DC-DCs see continuous barrier stress

General-purpose DC-DC converters are often specified with high insulation breakdown voltage and safety agency certifications but are only rated for occasional voltage stress and are expected to see little voltage across their barrier in operation. In high-side gate drive applications, however, the voltage across the barrier may be kV, switched at 100kHz or more with fast edges, over 100V/ns. This stress can lead to unreliable operation and short life of the DC-DC if not specifically designed for the job.

An operational consideration is barrier capacitance: often, general-purpose DC-DCs measure around 100pF but with this value, according to I = C.dV/dt, our 100V/ns edges would pump a massive 10A through the barrier into the control circuitry and back to the power switches through an indeterminate route. The effect would be increased EMI at best and at worst chaotic operation and damage. Barrier capacitances should therefore be a few pF maximum.

Avnet-Abacus-High-Side-Gate-Drives-EN-Image
Figure 2: Current and voltage transients in high-side gate drives

Even with low capacitance, the barrier of DC-DCs in the application is subject to a high electric field with implications for long term reliability. A phenomenon known as ‘Partial Discharge’ (PD) is a measure of the degradation of insulation when subject to high electric field strength. PD is caused by the gradual and sequential breakdown of micro voids in insulation leaving them carbonised and conductive. As more voids break down, the remaining insulation is subject to yet higher field strength leading to eventual run-away and total failure. PD has a definite ‘inception’ voltage below which no breakdown occurs and a lower ‘extinction’ voltage. In DC-DCs designed for high-side gate drives, the inception voltage should exceed the normal operating voltage by a good margin to indicate that long-term degradation will not be a problem. Testing for PD is complex and dedicated equipment is necessary that can detect inception, typically at several kV, with discharges measured in pico-coulombs.
 

PD testing proves long-term reliability

Manufacturers of DC-DCs such as Murata have done extensive testing for PD on their products, both on general-purpose types and those intended for high-side gate drive applications. Some test results are shown in Figure 3 for Murata parts showing worst-case inception voltages well over 3kV for their MGJ series, designed for gate drive applications.

The NCM6 series shows lower inception values even though it has high levels of safety agency rating, demonstrating that PD and safety rating are not necessarily correlated. The difference in this case being the construction of the barrier – the MGJ series is solid material whereas the NCM6 is multilayer.

 

 

Avnet-Abacus-PD-test-results-on-Murata-DC-DCs-EN-Image
Figure 3: PD test results on Murata DC-DCs
 

In many instances, the DC-DC converter needs low capacitance, good PD performance and a safety agency rating as well. The control circuitry is often accessible to touch through interfaces, for example, and the DC supply to the power switches could be several kV. Safety rules therefore apply and the DC-DC needs to have reinforced isolation, mandating creepage and clearance distances and an adequate insulation system. For industrial systems utilising three-phase high voltage supplies, the requirements can be extreme – for example 690VAC systems need 14mm creepage for compliance with the common standard EN 61800-5 for safety in motor drives.

Murata features high-side gate driver DC-DCs in its portfolio at power levels from 1W to 6W, including parts with multiple isolated outputs for all high side drives in half, full and three phase bridges. All DC-DCs hold safety agency certifications including a 6W part with 14mm creepage for 690VAC reinforced isolation. Download the brochure to find out more.

Aimtec also has solutions at the 2W power level with high operating temperature to 105°C.

If you need advice on selecting the right DC-DC converter for your application, or would like to discuss your full design in more detail, click the Ask an Expert button to get in touch with our team of technical specialists in your local language. Alternatively, click here to explore our range of DC-DC solutions and find further resources to support your design.

Want more like this? Sign up for our newsletters

About Author

Philip Lechner Photo
Philip Lechner

Philip Lechner studied electronics and telecommunications in Amsterdam before beginning his career i...

How to choose the right DC-DC converter for HV gate driver applications | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

How to choose the right DC-DC converter for HV gate driver applications | Avnet Abacus

Display portlet menu
Related Articles
Solar panels on a solar farm at sunrise
MOSFET relays: Key components in the densification and efficiency of electronics
November 27, 2019
Traditional electromagnetic relays, (EMRs), are still popular choices for certain applications, particularly where high-power switching is required, but increasingly, MOSFETs are being used in modern applications.
A photo of various antennas laid out on a white background
4 keys to selecting antennas for small IoT devices
November 19, 2019
Wireless connectivity is a critical enabler for many IoT applications. While a wireless module can simplify the RF subsystem design, a working system requires careful selection of an antenna as well.
Bigger is always better, isn’t it? That’s not necessarily the case when it comes to specifying a power supply.
AC-DC power supply design: how to specify capacity
January 15, 2020
AC-DC power supply design - how to pick an AC-DC power supply, and 80 PLUS Certification in context
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
These 8 charts will challenge your perspective on the Industrial IoT
October 1, 2019
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
Maximise your IIoT installation success by choosing the right sensors
July 19, 2019
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
Andy Hutton investigates the problems that LED flicker can cause in day-to-day life and the steps designers can take to prevent it in their lighting applications.
What is LED flicker - and how to prevent it
By Andrew Hutton   -   January 9, 2019
Andy Hutton investigates the problems that LED flicker can cause in day-to-day life and the steps designers can take to prevent it in their lighting applications.
ENEC (European Norms Electrical Certification) is the European hallmark for luminaires and related products and is used to demonstrate compliance with European safety standards. This certification system also includes LED drivers
Designing safe certified and efficient power solutions for LED lighting system
By Philip Lechner   -   November 22, 2018
ENEC (European Norms Electrical Certification) is the European hallmark for luminaires and related products and is used to demonstrate compliance with European safety standards. This certification system also includes LED drivers - the electronics th
Rapidly increasing market demand and the rationalisation of product offerings from Li-ion cell manufacturers are impacting the choices available to design engineers.
Strategies to combat volatility in the lithium-ion battery market
By Tim Parker   -   November 22, 2018
Rapidly increasing market demand and the rationalisation of product offerings from Li-ion cell manufacturers are impacting the choices available to design engineers. Here Tim Parker discusses the background to these dynamics and how engineers can suc
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
DC-DC power conversion challenges in transportation applications
By Andrew Hutton   -   November 22, 2018
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
When configurable power supplies are the best solution
By Hector Garcia   -   November 20, 2018
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
How wireless power transfer can help make the world’s lithium go further
By Martin Keenan   -   September 19, 2017
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
The market for consumer robots aimed at learning and education is growing rapidly, but selecting the right battery can make or break a companion robot's design.
Consumer robot designs present a challenge for Li-ion batteries
By Tim Parker   -   September 18, 2017
The market for consumer robots aimed at learning and education is growing rapidly, but selecting the right battery can make or break a companion robot's design.
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
Automotive telematics become mandatory with eCall
By Alan Jermyn   -   August 1, 2017
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Meeting regulatory requirements for mission-critical and non-mission-critical rolling stock power supplies
By Philip Lechner   -   June 13, 2017
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Hybrid capacitors combine technologies to get the best of both worlds
By Martin Keenan   -   March 15, 2017
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
Design considerations for powering remote bluetooth beacons
By Tim Parker   -   February 9, 2017
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
As LED luminaires have continued to develop in complexity and range and the number of different fixtures on the market has increased, lighting designers have begun to demand more flexibility from their driver hardware.
Programmable drivers add flexibility to LED lighting
By Don Schriek   -   December 8, 2016
As LED luminaires have continued to develop in complexity and range and the number of different fixtures on the market has increased, lighting designers have begun to demand more flexibility from their driver hardware.
If the feedback circuitry in a secondary-side regulated flyback converter could somehow be integrated into the switcher IC while maintaining isolation, the circuit would use fewer components and be smaller, simpler and cheaper overall.
Simplifying SMPS design with the right switching IC plus easy custom magnetics
By Philip Lechner   -   November 5, 2016
If the feedback circuitry in a secondary-side regulated flyback converter could somehow be integrated into the switcher IC while maintaining isolation, the circuit would use fewer components and be smaller, simpler and cheaper overall.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Since the 1990s, the external power supply has become the target of a series of regulations that are gradually being tightened around the world.
The power regulations spiral
By Andrew Hutton   -   May 24, 2016
Since the 1990s, the external power supply has become the target of a series of regulations that are gradually being tightened around the world.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Specifying medical power supplies can be particularly challenging because of the standards and jargon surrounding this application.
Deciphering datasheets for medical PSUs
By Philip Lechner   -   April 29, 2016
Specifying medical power supplies can be particularly challenging because of the standards and jargon surrounding this application.
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Design trends: Batteries for IoT
By Tim Parker   -   March 11, 2016
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Lithium batteries have been in the news again recently, unfortunately for all the wrong reasons.
How to impose a smoking ban on lithium batteries
By Tim Parker   -   July 9, 2015
Lithium batteries have been in the news again recently, unfortunately for all the wrong reasons.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Keenly associated to the trend of greater computing power and complexity is a technology that is making a move into industrial from the communications field: that of advanced power system architectures.
Advanced power architectures move into industry
By Philip Lechner   -   April 20, 2015
Keenly associated to the trend of greater computing power and complexity is a technology that is making a move into industrial from the communications field: that of advanced power system architectures.

How to choose the right DC-DC converter for HV gate driver applications | Avnet Abacus

Display portlet menu
Related Events
TechTrends 2020
Date: February 19, 2020
Location: Duiven
Embedded World 2020
Date: February 25, 2020
Location: Nuremburg, Germany