4 Keys to Selecting Antennas For Small IoT Devices | Engineers' Insight | Avnet Abacus

Display portlet menu

4 Keys to Selecting Antennas For Small IoT Devices | Engineers' Insight | Avnet Abacus

Display portlet menu

4 keys to selecting antennas for small IoT devices

A photo of various antennas laid out on a white background

Wireless connectivity is a critical enabler for many IoT applications, particularly those that need to be mobile, or where cabled data communication is not cost-effective or practicable. Popular wireless protocols include Bluetooth®, ZigBee®, and Wi-Fi®, which operate in the 2.4GHz or 5GHz frequency band and can sustain high data rates over relatively short range. Standards such as LoRa and Sigfox support connections over longer distances, at lower data rates, operating in sub-GHz bands (868MHz in Europe).

Designing an RF subsystem based on any of these protocols demands specialist skills, often most readily sourced by adopting a wireless module or a reference design that comes with protocol stacks already integrated and critical hardware-layout issues solved. While these can greatly simplify design challenges, achieving a working solution is not an easy plug-and-play enterprise.
 

1. The system is the antenna

Among the challenges that must be dealt with, selecting and integrating a suitable antenna has a significant impact on the RF-subsystem and consequently affects the system performance in terms of communication range, overall power consumption, and battery life.

The antenna is often required to fit inside the device enclosure, which usually demands small size and careful positioning to ensure optimal performance. On the other hand, a suitable antenna should also have high efficiency and adequate bandwidth covering the desired frequency range.

Improving any of this triad of parameters is achieved at the expense of the other two. Hence implementing a suitable antenna calls for compromise, using the datasheet figures only as a guide to performance in the final application. Factors such as the antenna connection, positioning relative to other components inside the enclosure, and the properties of the enclosure material and any coatings that may be applied to it, also have noticeable effects.  

For these reasons it is best to consider antenna design issues as early as possible in the project, on the basis that, from an overall RF performance standpoint, the entire system is the antenna.
 

2. Integrating a 2D or 3D antenna

Figure 1: Effective use of ground plane allows a smaller antenna

A discussion of antenna basics will show that a centre-fed dipole antenna should have length equivalent to one half of the wavelength of the signal, to achieve resonance. A combination of a smaller monopole antenna, one-quarter wavelength long, close to a ground plane connected as a return path, has a comparable effect; ideal for space-constrained IoT devices. The ground plane effectively creates an image of the monopole conductor (Figure 1), and so must be adequately sized.

A simple quarter-wavelength wire antenna could be arranged in free space above the PCB, fed by a transmission line designed to match the RF-amplifier output impedance. In practice, miniaturised PCB antennas are better suited to volume production. Typically featuring an inverted-F, L-shaped, or meandered antenna pattern, they are reliable, easy to use, and adjustment-free.

A PCB antenna can be attached to the main circuit board, above the ground plane. The ground plane must be the top layer of the main circuit board, and the design must respect the “keep out” areas specified in the antenna datasheet.

PCB antennas are intended to be mounted at the edge of the circuit board. If space constraints inside the enclosure demand more flexibility in positioning the antenna, a PCB antenna can be connected to the main board using a miniature coaxial cable and U.FL connector. A stamped metal antenna is a suitable alternative, particularly if high-volume, high-speed assembly is a priority. If space is extremely limited, three-dimensional antennas made using moulded interconnect device (MID) technology can be considered.

Although an antenna can be selected to have the same impedance as the RF-amplifier output, loading by nearby components on the circuit board and the material properties of the device enclosure may require a matching network to be inserted. This can be a simple single series capacitor and parallel inductor for a single-band antenna, or a more complex network for a dual-band application (Figure 2).

An impedance matching circuit may be needed to maximise power transfer

3. Ensure timely delivery of custom antenna

A standard antenna capable of meeting the system performance requirements usually offers the most cost-effective solution, benefiting from easy and fast off-the-shelf availability. On the other hand, if size constraints are extremely tight or performance targets extremely high, a custom antenna may be needed. To ensure timely delivery, consulting suppliers early is recommended. The supplier needs to know the frequency bands bandwidth, efficiency, link budget, and any multiband requirements.
 

4. Plan for RED and EMC compliance

Wireless IoT devices to be marketed in Europe must comply with the recently introduced Radio Equipment Directive (RED) as well as the EU Electromagnetic Compliance (EMC) Directive. As far as EMC is concerned, high-frequency circuitry such as switching regulators powering various parts of the system, or an unintentional radiator such as a current loop, can cause problems. If EMC is left as an afterthought, common techniques applied as a quick fix – such as board-level shielding – can significantly impair the antenna’s performance.
 

Conclusion

A variety of standard antennas that are designed for frequencies appropriate to IoT applications, and also are compatible with the extreme size and power constraints that apply to typical IoT endpoints, is available. Nevertheless, successfully integrating an antenna is not a simple plug-and-play exercise, and requires careful selection, awareness of the effects of other components in the system, including the enclosure, and fine-tuning of the antenna feed and positioning.

It is worth keeping an eye on technical developments, too. In the quest to usurp the trade-off between miniaturisation, efficiency, and bandwidth, researchers are investigating advanced materials such as graphene – leveraging its excellent conductivity to print thin and flexible antennas, dielectrically loaded polymers, and textile antennas for wearable applications.

To learn more about selecting and integrating an antenna suitable for small-size IoT devices, download the TE Connectivity wireless white paper, or if you would like to discuss your design in more detail, click the Ask an Expert button to get in touch with one of our technical specialists in your local language.

Want more like this? Subscribe to our newsletters

4 Keys to Selecting Antennas For Small IoT Devices | Engineers' Insight | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Webinar: Antenna design and integration for Industrial IoT applications

-
On-demand

This webinar will provide an in-depth analysis of antenna technology, addressing the important factors to consider when choosing a solution, as well as tips on understanding datasheets.

White paper

Wireless options for the Industrial IoT

Learn about the key design challenges that affect antenna and protocol selection, as well as the different antenna types and the advantages and disadvantages of each, so you can ensure your wireless system performance is never compromised.

4 Keys to Selecting Antennas For Small IoT Devices | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Articles
Solar panels on a solar farm at sunrise
MOSFET relays: Key components in the densification and efficiency of electronics
November 27, 2019
Traditional electromagnetic relays, (EMRs), are still popular choices for certain applications, particularly where high-power switching is required, but increasingly, MOSFETs are being used in modern applications.
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
These 8 charts will challenge your perspective on the Industrial IoT
October 1, 2019
As the buzz around the Industrial IoT continues to grow, are manufacturers ready to move beyond the hype? How close are we to extensive IoT implementation and delivering real business value?
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
Maximise your IIoT installation success by choosing the right sensors
July 19, 2019
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
A quick guide to multi-standard mesh networking
By Alessandro Mastellari   -   April 11, 2019
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.
How to choose the right DC-DC converter for HV gate driver applications
By Philip Lechner   -   January 31, 2019
Learn about the key design considerations and technical trade-offs that you need to know when selecting DC-DC conversion solutions for inverter or motor control HV gate drivers.
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
A quick guide to powering smart objects with kinetic energy harvesting
By Alessandro Mastellari   -   January 22, 2019
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
When configurable power supplies are the best solution
By Hector Garcia   -   November 20, 2018
Traditionally, system designers try to use ‘off-the-shelf’ standard components, expecting the lowest cost as a result. With power supplies, this is not necessarily the case when a holistic view is taken. A compelling case can be made for cost eff
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Security and surveillance: Two sides of the coin in smart homes
By Martin Keenan   -   July 9, 2018
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Future proofing lighting systems with Bluetooth
By Alessandro Mastellari   -   May 9, 2018
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Optimising battery designs with supercapacitors
By Tim Parker   -   April 30, 2018
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
From enabled to proactive: The evolution of home automation
March 29, 2018
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Adapting PIR sensor technology to new applications
By Martin Keenan   -   February 7, 2018
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
State-of-the-art wireless modules save time, space and money
By Martin Keenan   -   September 12, 2017
Thanks to the emergence of the internet of things (IoT), almost all of today’s electronic device designs will have to integrate some form of wireless connectivity or other. The easiest, quickest and cheapest way to do this is with wireless modules.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Datacentre racks
Chip-to-chip at the speed of light
By Marco Enge   -   March 31, 2017
As data centres and data farms continue to expand and grow, better solutions are required for system architectures that allow faster communication and more efficient operation.
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Hybrid capacitors combine technologies to get the best of both worlds
By Martin Keenan   -   March 15, 2017
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
Design considerations for powering remote bluetooth beacons
By Tim Parker   -   February 9, 2017
There are a number of battery form factors and chemistries available for powering remote beacon technology. In this article, Avnet Abacus’ Tim Parker guides you through the available options.
As one of the world’s leading manufacturers of wireless modules for smartphones, including supplying some of the very biggest names in the market, Murata knows a thing or two about wireless technologies, and also about manufacturing modules.
Designing for LoRaWAN - Murata wireless modules
By Martin Keenan   -   December 1, 2016
As one of the world’s leading manufacturers of wireless modules for smartphones, including supplying some of the very biggest names in the market, Murata knows a thing or two about wireless technologies, and also about manufacturing modules.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Bluetooth Beacons and NFC (Near Field Communication) are often mentioned in the same breath, but in terms of technology and applications, they are not really that similar.
NFC vs. Bluetooth beacons: More different than similar
By Martin Keenan   -   August 12, 2016
Bluetooth Beacons and NFC (Near Field Communication) are often mentioned in the same breath, but in terms of technology and applications, they are not really that similar.
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Selecting fibre optic cables
By Marco Enge   -   July 12, 2016
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Specifying medical power supplies can be particularly challenging because of the standards and jargon surrounding this application.
Deciphering datasheets for medical PSUs
By Philip Lechner   -   April 29, 2016
Specifying medical power supplies can be particularly challenging because of the standards and jargon surrounding this application.
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
The internet of medical things (IoMT) bringing better healthcare for all
By Martin Keenan   -   April 8, 2016
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Design trends: Batteries for IoT
By Tim Parker   -   March 11, 2016
Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.
Battery charging without cables can add convenience, durability and safety to a number of different applications.
A quick introduction to wireless charging
By Alan Jermyn   -   November 20, 2015
Battery charging without cables can add convenience, durability and safety to a number of different applications.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.

4 Keys to Selecting Antennas For Small IoT Devices | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Events
TechTrends 2020
Date: February 19, 2020
Location: Duiven
Embedded World 2020
Date: February 25, 2020
Location: Nuremburg, Germany