|
|
|
|
|
|
|
|
|
screenshots |
| PCItree |
PCItree displays all components of the PCIbus as a tree structure. The Config Space of devices can be read and edited. If a device features io or memory space it can be read and edited as well (but be carefull! it can hang or even damage your hardware!).
last PCI bus number: The value
of the highes PCIbus number is displayed
right above the tree
pane
b.d.f : Each PCI component has an integer number for bus, device and function.
direct select: in case you
think not all components in the PCIbus system are found:
any b.d.f can be choosen
directly by the three spin controls in the
direct select box. A
config read is done for this b.d.f and the result is
displayed in the Config
Space Dump.
If for a choosen b.d.f
a PCI component exists it is highlightet in the tree pane.
++ expands all levels
of the tree
-- collapses all levels
of the tree
refresh tree rescans
the whole PCIbus
save tree writes the
tree structure to a file
reset bridge
resets the secondary PCIbus of a PPB
Nr of ConfRegs:
16 : config space from
adress 0 to 0x3f is read (default)
64 : config space from
adress 0 to 0xff is read
refresh dump
: rereads the config space of the device and displays it
If a component is selected
in the tree the register contents of its configuration
space (16 or 64 dwords) are
displayed in the lower right window.
If a BAR is used (value !=
0) it is indicated wether its memory or io space.
You can
double click on a BAR
to view/edit the memory/io space
You should know what
happens if you read memory/io space !!
The following information
is extracted and decoded from the config space:
VendorID:
value & decoded
DeviceID:
value
Subsys VID:
value & decoded
Subsys ID :
value
Base/Sub Class code:
value & decoded
Interrupt Pin/Line:
decoded
revision number:
value
you can click and double click on a Config Space Register in the list box
if you click on a Config register
in the list box its DWORD contents is displayed
in the edit box. You can modify
this value (the 1st character must be an x). The
string will be scanned by
sscanf(str, "x%X", &data).
Write ConfReg writes the DWORD
value of the edit box to the Config register.
The sscaned value is
displayed below the edit box (for feedback).
refr after wr. refreshes the dump after the Write Confreg
A component with a INT pin
is displayed as "X(b.d.f)DDDD.VVVV" where X is one of
the INT pins INTA to INTD.
b.d.f is bus.device.function number. DDDD is DeviceID
and VVVV is VendorID.
Note: the range of the BAR
space is not derieved because it needs a READ-WRITE-READ-
WRITE sequence to the BAR
which can cause malfunctions of the PCI system !!
(see "BAR space" below)
Only 32 bit adress space is supported.
BAR space detection:
If you click YES in
the message box the following happens:
the BAR in the ConfigSpace
is read and stored
the BAR is written
with 0xffffffff (!!)
the BAR is read. With
the read value the size of the memory/io space is determined
the BAR is written
with the stored BAR value
a linear adress of
1Kbyte is mapped to the physical adress (the contents of the BAR)
a new Dialog window
with a list box is opened
(In some cases
the described BAR detection can cause malfunctions of the PCI system because
the BAR is temporarily changed !!)
If you click NO then
the described procedure is not done. Instead a size of 1 MByte is assumed.
Display range:
128 Bytes: only
the first 128 Bytes of the selected 1Kbyte range are displayed
and refreshed
(faster cont. cycles & shorter cycles to
view with a logic
analyzer)
1024 Bytes: the
whole 1K range is displayed in the list box (default)
If the size of the memory/io space is smaller only this space is displayed.
select view range:
If the size of the
memory/io space is bigger than 1Kbyte then you can select another
1Kbyte block to be
displayed in the list box. Just move the scrollbars for KB range
and MB range.
list box contents:
1st col: DWORD contents
(MSbyte:LSbyte)
2nd col: address offset
in the memory/io space
3rd col: ASCII character
of the 4 bytes (LSbyte:MSbyte)
refr. view
: rereads the selected 1Kbyte (or 128 Byte) block and displays it in the
list box
the first DWORD of the selected
range is displayed in the edit box.
Physical address and number
of selected DWORDs are displayed at the right of the edit box.
You can modify the value in
the edit box (the 1st character must be an x). The
string will be scanned by
sscanf(str, "x%X", &data) when the write button is pushed.
The sscaned value is displayed
below the edit box (for feedback).
Write Memory writes the DWORD
value of the edit box to the selected range with
the following options:
loop on/off. continously
loops accesing the selected range
stops if button is
being unchecked
toggle. toggles
(inverts) every second DWORD to be written
count. increments
each WORD of the DWORD for the next write access
verify. after the selected
range is written it is read and compared to the
written values. If
an error occurs (the cont. loop is stoped and) the
false values are highlighted
in the list box
refresh view after write.
refreshes the whole list box after the selected
range is written (and
verified)
the function memcpy( p_dest,
p_src, b_range ) is used to read max. 1Kbytes
from the selected memory/io
space to a buffer and then write it to the
selected destination.
memcpy is expected to use faster PCI transfers (bursts).
possible problems to get the
BAR space:
----------------------------------------
> To: Mailing List Recipients
<pci-sig-request@znyx.com
> cc: (bcc: Michael
Reusch/FAST Multimedia AG)
> Subject: Re: Unruly BIOSes
and the Intel i960RP
>
>
>
> I had a problem with
a Base Address Register in the Intel i960RP. The
> BIOS writes FFFF FFFF
to this register and then reads what comes back to
> determine the size required
by the device. The i960 returns a value
> based on the limit register
once and once only, and subsequent reads
> from the BAR return the
current programmed value of BAR. The PCI
> specification, as I read
it, does not preclude this behaviour.
>
> It would seem to be more
complicated to implement this behaviour as it
> requires a register to
keep state information, and a side effect of
> reading in configuration
space is to alter this state. Still, that is
> what happens, so I have
to live with it.
>
> Some BIOSes, it seems,
read the BAR twice when determining the address
> limit. Such BIOSes are
confused by what they see come back, and so write
> 8000 8000 to the BAR.
This seems to me equally bizarre. Surely 0000 0000
> would be a more sensible
thing to write to a difficult BAR: this would
> effectively disable the
allocation requested by that BAR ?
>
> I am considering writing
a PCI configuration helper which runs after the
> BIOS but before Windows
gets started, and straightens out anomolies such
> as the one above.
>
> Any thoughts?
>
>
> Roy Gwinn.