SRAM芯片

SRAM (Static random-access memory) is a type of random access semiconductor memory which is a volatile memory (meaning that its data is lost when power is turned off) and stores each bit of data generally in flip-flops. So the frequent refreshing activity is not required unlike in DRAM. As long as power is there, data will be retained without refresh. One SRAM memory cell contains 6 transistors (four transistors configured as two cross-coupled inverters and additional two transistors to control the access to the memory cell). A basic SRAM provides fast data access but holds less data per unit volume so are more expensive than DRAM. So It is commonly used in cache memory, video card memory etc.

查看全部
添加到物料清单
添加到新的物料清单
您的物料清单
关闭
该项目将被添加到您的“精确匹配”
关闭
发送此页面的链接
Please enter a valid Email id
链接
Sender# Invalid address error message
发送到
jsmith@baa.com
sjohnson@baa.com
添加另一个地址
添加另一个地址
添加另一个地址
主题
留言

匹配结果

匹配结果 清除所有过滤器