DRAM芯片

DRAM (Dynamic random-access memory) is a type of random access semiconductor memory which is a volatile memory (meaning that its data is lost when power is turned off) and stores each bit of data in a separate tiny passive electronic component (such as capacitor) inside an integrated circuit. DRAM usually consists of one capacitor and transistor per data bit. Each electronic component has two states of value in one bit called 0 and 1 (like capacitor can either be charged or discharged; these two states are generally considered as 0 and 1). The capacitor starts to discharge slowly if there is no intervention, so the data on the chip also fades with the discharge. Capacitor need to be refreshed frequently to prevent this discharge so an externa refreshing circuit is needed to restore them to their actual charge and rewrite the data. Because of this frequent refreshing activity it is called as a dynamic memory. DRAM is used for frequent access and temporary data storage. DRAM is widely used where low-cost benefits and high-capacity memory is required. DDR (Double Data Rate) memory is the most commonly used DRAM memory and DDR4 is the latest generation of DDR. Also LPDDR is used for applications such as mobile and embedded boards where low power is concerned

查看全部
添加到物料清单
添加到新的物料清单
您的物料清单
关闭
该项目将被添加到您的“精确匹配”
关闭
发送此页面的链接
Please enter a valid Email id
链接
Sender# Invalid address error message
发送到
jsmith@baa.com
sjohnson@baa.com
添加另一个地址
添加另一个地址
添加另一个地址
主题
留言

匹配结果

匹配结果 清除所有过滤器