Custom Meta Tags

Category Attributes

Category Attributes

電源和充電

  篩選條件   電源和充電 RSS FEED
Wireless charging is everywhere. From airports to automobiles, and hotels to offices—designing the right charging solution can be complex. Explore our resources to get technical expertise and stay up to date with charging trends and technology.
Conceptual image of smart car in purple
Advances in charging infrastructure drive the rise of green mobility
2024年5月15日
Advances in charging infrastructure, EVs’ “energy supply station”, are directly related to the market growth of the vehicle of the future.
Conceptual image of smart car in purple
Home energy storage systems in the shift to green energy
2024年2月15日
As technology continues to advance and the market matures, home energy storage systems will play an increasingly important role in the future.
Conceptual image of smart car in purple
Industrial energy storage for a sustainable future
By Avnet Staff   -   2023年8月15日
Energy storage is the most critical and challenging factor in the energy production and utilization chain. As it has a critical impact on energy efficiency, it is the focus of intensive research and development.
Industrial cloud platforms, the engine that improves quality and performance
Wireless charging will set us free!
2023年5月15日
As technology continues to advance and consumers demand more convenient and efficient charging solutions, wireless charging will become an integral part of our daily lives. As development efforts intensify, all minor obstacles will no doubt be overco
Medical worker puts a smartwatch used for remote monitoring on a patient’s wrist
Diagnostic wearables: Design challenges and opportunities
By Karen Field   -   2023年2月15日
From the need to maintain small form factors and keep system power requirements low to concerns over data integrity and cost, the design space for diagnostic wearables is fraught with complexity.
Smart watch worn on a wrist showing pulse rate.
Are wearables the killer app for energy harvesting technology?
By Karen Field   -   2022年10月13日
As wearable devices grow in popularity, so does interest in energy harvesting technology as an alternative to battery power. Experts say it shouldn’t be an “all-or-nothing: proposition.
Solar and wind farm
Energy Transformation in the Low-Carbon Era: Harnessing the power of Renewable Energy
2022年9月15日
The dynamic development of new energies, such as photovoltaics, is essential to achieving carbon peaking and carbon neutrality goals.
Solar and wind farm
Batteries won’t do for renewable energy storage
By Cameron Coward   -   2022年9月15日
Solar and wind energy has a serious drawback: it isn’t always available on-demand. These methods enable renewable energy storage that can meet demand throughout the day and night.
Point at a beating heart
How Cold, Lifeless Machines Can “See” Our Colorful and Complex World?
2022年8月17日
In the wave of AI, IoT, cloud computing, and smart sensor technology, machine vision may become humanity’s “third eye”, giving people a glimpse into the yet unseen future world of “everything is connected, everything is smart.”
Point at a beating heart
What is the “alien” material silicon carbide worth today?
2022年7月17日
The potential for improving the performance of silicon-based devices is limited. Many manufacturers have been forced to increase the size of their devices to improve performance.
EV charging station
Designing ultra-rapid DC EV chargers
2022年7月13日
If electric drivetrains are to replace internal combustion, particularly in larger vehicles, we need more high-speed DC charging capacity. This article examines six of the main design considerations.
Person paying for EV charging with a credit card
Defining security for the EV charging infrastructure
2022年7月13日
Drivers are demanding easy access to public EV charging points. Providers must meet this demand without sacrificing security for simplicity. Cybercriminals will find any security weaknesses, but the latest standards are here to help.
Electric bus at EV charging station
Predicting the kW sweet spot in EV charge point variants
2022年7月13日
Do you want AC or DC, fast or slow charging? Manufacturers of Electric Vehicle Supply Equipment need to predict what will be demanded most by consumers, while responding to the requests coming from Charge Point Operators.
Electric car being charged
Load balancing in the EV charging infrastructure
2022年7月8日
We all know what it’s like to wait in line to refuel, but what if you must continue waiting after you plug in your EV? Managing multiple charge points in one location is creating some interesting challenges for the EV charging infrastructure.
WBG motor control
Selecting wide bandgap devices for motor control applications
By Milan Ivkovic   -   2021年12月20日
When it comes to smart control applications, it’s worth taking a step back to consider when and if the switch to wide bandgap from MOSFET or IGBT makes sense. When the answer is yes, then the decision is whether SiC or GaN is the way to go.
A group of colleagues working in a computer security room having a discussion
Just how Fast is EV “Fast Charging”?
2021年11月15日
Drivers of electric vehicles are a diverse bunch, but they are united by two questions: How far can my car go? and Where can I charge?...Today, we will be talking about that specific concern—electric vehicle (EV) charging.
man holding tablet computer
When will wireless power transfer redefine the Industrial IoT?
2021年11月12日
Power loss in a single sensor might result in downtime for an entire production line, so keeping them operational will be critical. With developments in the enabling technologies, could wireless power transfer be the answer?
woman navigating a smart car dash pad
Advances in wide-bandgap semiconductors for vehicles
By Jason Struble   -   2021年8月24日
See the technical and cost comparisons between older silicon IGBT and MOSFET technologies and newer generation silicon carbide switches.
electric vehicle charging station sign
EV charging: The drive for faster charging speeds and higher efficiency
2021年8月11日
Fast DC chargers and wide-bandgap silicon carbide switches are key to improved EV charging.
Li-ion battery
To fight EV fires, focus is on early detection of battery cell thermal runaway
2021年8月11日
Sensing solutions that focus on decomposition gases are being used to focus on early detection of battery cell thermal runaway.
Electric Vehicle recharging
As EV market grows, so does push for higher efficiency
2021年8月11日
‘The electric car has no future.’ That’s what some said in 1908 when Henry Ford introduced his cheap Model T. Despite his new assembly line manufacturing concept, that single statement rendered electric vehicles (EVs) obsolete. EVs had been around since...
A group of colleagues working in a computer security room having a discussion
Electric cars are all vying for SiC...but why?
2021年7月15日
In addition to inverters, SiC power devices can also be used in many aspects, such as on-board chargers (OBC) and power conversion systems (DC/DC) of electric vehicles.
Cleanroom tech with wafer
Three design freedoms enabled by SiC technology
By Milan Ivkovic   -   2021年4月17日
Even with the undeniable performance and potential of silicon carbide (SiC) technology, some designers may be hesitant initially to tackle new projects using SiC.
lab techicians
The undeniable advantages of SiC technology over Si
By Milan Ivkovic   -   2021年4月16日
Silicon carbide (SiC) technology has reached the tipping point, the state when undeniable advantages push a technology into rapid adoption.
lab techicians
The undeniable advantages of SiC technology over Si
By Milan Ivkovic   -   2021年4月16日
Silicon carbide (SiC) technology has reached the tipping point, the state when undeniable advantages push a technology into rapid adoption.
A group of colleagues working in a computer security room having a discussion
Does anyone make “fever cooling pads” for data centers?
2020年9月1日
In this era of IoT we all suffer to varying degrees from power shortage anxiety. We find ourselves constantly worrying about whether our "smart" mobile phones, bracelets, door locks and other devices can be sufficiently powered.
A group of colleagues working in a computer security room having a discussion
What kind of "charger” will improve the battery life of TWS headsets?
2020年9月1日
TWS headsets have maintained a 100% growth rate in the past few years. Shipments reached 120 million units in 2019, and are expected to exceed 200 million units by the end of 2020.
2D image of smart phone charging on mobile battery
Why does Iq matter for USB Type-C?
2019年11月11日
This change is driving an increase in demand for Type-C AC/DC chargers and power banks because the Type-C connector has flip capability which gives convenience to users.
avnet branded USB type C connector
It is time to say goodbye to Micro USB!
2019年11月11日
Type-C’s greatest advantage is its integration capability. In addition to not having a right or wrong side (a perennial problem for Micro USB users), Type-C is able to offer integrated power delivery (PD) during charging.
Using Programmable Logic to Build Power-Efficient Systems
2019年10月29日
The successful implementation of the Internet of Things (IoT) requires new thinking about how to power connected devices.
First1 2Last  Results Per Page: 30 6090All      

Category Attributes

培训与活动
関連イベントはありません

Category Attributes

电源及充电

  筛选条件   电源及充电 RSS FEED
Wireless charging is everywhere. From airports to automobiles, and hotels to offices—designing the right charging solution can be complex. Explore our resources to get technical expertise and stay up to date with charging trends and technology.

Featured

Conceptual image of smart car in purple
充電インフラの整備で持続可能な技術発展を牽引
2024年5月15日
そして、EV(電気自動車)の「エネルギー補給場所」である充電インフラは、その技術の奥行きと成熟度が、EVの普及と応用を直接左右します。

Featured

風力発電と貯蔵システム
グリーンエネルギーへの転換期にある家庭用蓄電システム
2024年3月6日
世界のエネルギー市場は重要な過渡期にあります。従来のエネルギー源、特に化石燃料は、環境に大きな影響を与えます。地球規模の温室効果ガス(GHG)の主な発生源であり、

Featured

Industrial Energy Storage for a Sustainable Future
持続可能な未来のための産業用エネルギー貯蔵
2023年9月7日
持続可能な開発についてどうお考えですか?グリーン化、再生可能資源へのシフト、環境保護、クリーンエネルギーの活用、リサイクルはすべて、持続可能な開発という...

Featured

かざしてチャージする
ワイヤレス充電は、私たちを自由にする!
2023年6月12日
IoT(Internet of Things)の進展に伴い、私たちはますますテクノロジーに依存するようになりました。あなたも充電ケーブルが絡まってしまったことがあるのではないでしょうか。

Featured

患者に医療用スマートウォッチを取り付ける医師
診断用ウェアラブル機器:設計課題およびチャンス
2023年3月3日
診断用ウェアラブル機器の設計分野は、小型化の維持、消費電力の抑制、データの整合性とコストに関わる懸念に至るまで、複雑さを極めています。

Featured

発電用の風車と太陽光パネル
低炭素時代のエネルギー転換:再生可能エネルギーの利用
2022年10月6日
1996年、ある生物学者が、通常は中国南部でしか見られないオオカバマダラ(モナーク蝶)が北部で目撃されたという事実をつかみました。

Featured

太陽光パネル
"宇宙から来た" 炭化ケイ素の現在価値は?
2022年8月11日
有史以来、人類は、新素材を絶え間なく探してきました。科学は、しばしば自然の摂理に挑んできました。

Featured

EVに急速充電中
EVの「高速充電」は、どの程度、高速か?
2021年12月3日
EVのドライバーは多様ですが、走行距離と充電場所に関する疑問点で一致しています。本日は、EVの充電という具体的な懸念に関してお話します。

Featured

EVを支えるSiC
EVがSiCを奪い合い…なぜ?
2021年8月11日
つい最近、ルノーグループとSTMicroelectronicsは、2026~2030年の新エネルギー車向けのSiC(炭化ケイ素)およびGaN(窒化ガリウム)製品の供給に関して提携協定を締結したと発表しました。

Featured

ワイヤレスヘッドフォンをして海辺で一休みする、運動中の女性
TWSヘッドフォンのバッテリー寿命を延ばす「充電器」とは?
2020年12月13日
IDCが発表した最新のデータによると、世界のウェアラブル端末の出荷台数は、2020年に前年比14.5%増の3億9600万台に到達する見込みです。ウェアラブル市場における全出荷台数の約60%は、ワイヤレスヘッドフォンが占めています。本当に見事です。 図1:世界のウェアラブル市場の出荷台数の分析(出典:IDC)   ワイヤレスヘッドフォンの需要を促す主な要因の1つは、TWS(完全ワイヤレスステレオ)ヘッドフォンの台頭です。アップルは2016年にAirPodsを発売し、ごく短期間に市場で大きな成功を収めまし...
man holding tablet computer
ワイヤレス電力伝送は、インダストリアルIoTの再定義につながるか?
2021年11月12日
センサーの稼働を維持することは非常に重要です。このような状況において、ワイヤレス給電は有効な手段なのでしょうか?
USB 3.0のコネクタ
Micro USBに終わりを告げる時!
2019年1月21日
USB Type-C + Power Delivery 3.0は、3Cとモバイル機器の充電を統合Appleが MacBookでType-Cの使用を開始して以来、大手メーカーは、自社の製品でUSB Type-C を採用してきました。またType-Cは、最大の
佇む電気自動車
バッテリーマネジメントシステムの大切さ
2018年10月3日
国際エネルギー機関(IEA)によると、電気自動車(EV)の数は、2016年に世界で200万台に達しました。さらに、EV市場は、2020年までに900~2000万台、2015年までに4000~9000万台に増加する見込
First1 Last  Results Per Page: 30 6090All